Search found 3 matches

by genhung
Wed Apr 04, 2012 9:56 am
Forum: Grove
Topic: Music Shield and Wiznet Ethernet shield
Replies: 5
Views: 3628

Re: Music Shield and Wiznet Ethernet shield

hi deray

If both Music Shield and Wiznet Ethernet shield need ISP interface for talking to MEGA,
When I joint these two shield together, will it cause conflicts???

Thanks
by genhung
Sat Mar 31, 2012 1:33 pm
Forum: Grove
Topic: Music Shield and Wiznet Ethernet shield
Replies: 5
Views: 3628

Re: Music Shield and Wiznet Ethernet shield

thanks deray
It sounds to me I can put Ethernet shield on the MEGA, then MUSIC shield on the Ether shield. Is it?
Is it fine for not connecting ISP (6pin::MISO\SCK\RST\VCC\HOSI\GND) to Music Shield??
Thanks again!
by genhung
Fri Mar 30, 2012 2:28 pm
Forum: Grove
Topic: Music Shield and Wiznet Ethernet shield
Replies: 5
Views: 3628

Music Shield and Wiznet Ethernet shield

Hi there,

I have just received the following items from Seeed Studio

(1) Music Shield (INT109B2P)
(2) Wiznet Ethernet shield -w5100 (ARD124B2P)

Are these two boards compatible to each other?
How can I joint them together onto an Arduino MEGA board?

Please help.