Search found 9 matches

by MikeHole
Fri Aug 21, 2015 9:03 pm
Forum: Wearables
Topic: Main Board V1.3 on Windows 10 - Keeping USB alive
Replies: 5
Views: 2291

Re: Main Board V1.3 on Windows 10 - Keeping USB alive

Ok everything is now working sorry spotted that the USB device disappears because it then reports to be an Arduino Leonardo ... After flashing my 1st program it reports to be a Xadow :) Also spotted that the installation includes the files to be dropped into the Arduino\hardware\seeeduino folder so ...
by MikeHole
Fri Aug 21, 2015 8:23 pm
Forum: Wearables
Topic: Main Board V1.3 on Windows 10 - Keeping USB alive
Replies: 5
Views: 2291

Re: Main Board V1.3 on Windows 10 - Keeping USB alive

just looking to see if I can upload a file to the device but I am geeing the following error when compiling:

USBCore.cpp:25:22: fatal error: Platform.h: No such file or directory

:roll:
by MikeHole
Fri Aug 21, 2015 8:12 pm
Forum: Wearables
Topic: Main Board V1.3 on Windows 10 - Keeping USB alive
Replies: 5
Views: 2291

Re: Main Board V1.3 on Windows 10 - Keeping USB alive

Trying this on a spare Dell Venue Pro 8 (it's all I have at the time) it installs as a Arduino Leonardo is this workable?
by MikeHole
Fri Aug 21, 2015 8:07 pm
Forum: Wearables
Topic: led module more than one
Replies: 5
Views: 2252

Re: led module more than one

What compiler would I use to recompile the code and can you recommend a programmer capable of writing to the chip via the pins?

Cheers,

Mike
by MikeHole
Fri Aug 21, 2015 4:09 pm
Forum: Wearables
Topic: Main Board V1.3 on Windows 10 - Keeping USB alive
Replies: 5
Views: 2291

Main Board V1.3 on Windows 10 - Keeping USB alive

Hi,

When I plug the main board into the USB on my machine it appears as "USB Serial Device (COM8)" but only stays connected for about 5 seconds.

Is there any way of making sure that the device stops doing this so that I can upload programs?

Cheers,

Mike
by MikeHole
Fri Aug 21, 2015 3:14 pm
Forum: Wearables
Topic: led module more than one
Replies: 5
Views: 2252

Re: led module more than one

:( so there is no way of changing code in the modules built-in microcontroller to change it's address at all?
by MikeHole
Fri Aug 21, 2015 5:00 am
Forum: Wearables
Topic: led module more than one
Replies: 5
Views: 2252

led module more than one

Is it possible to connect two led modules and control them independently?
by MikeHole
Fri Mar 23, 2012 4:50 pm
Forum: Grove
Topic: Keypad Module - Netduino
Replies: 2
Views: 2605

Re: Keypad Module - Netduino

I do thanks but this is information I know already :( I have an active post on the netduino forum if anybody will be able to help: http://forums.netduino.com/index.php?/topic/3790-seedstudio-keypad-module/page__gopid__25886#entry25886 Thanks for your help in this I know this is all the information t...
by MikeHole
Thu Mar 22, 2012 9:34 pm
Forum: Grove
Topic: Keypad Module - Netduino
Replies: 2
Views: 2605

Keypad Module - Netduino

I recently purchased the Electronic Brick Starter kit for use on my Netduino Plus board. Loving the experience so far :). I also purchased the Keypad Module (BUS) http://proto-pic.co.uk/electronic-brick-keypad-module-bus/ not realising that this is a discontinued product  I have tried to work out h...