Search found 7 matches

by dan295
Thu Aug 01, 2019 1:55 pm
Forum: Shields
Topic: Activate is failed when using P2P_Push sample sketch with NFC Shiled V2.1
Replies: 0
Views: 680

Activate is failed when using P2P_Push sample sketch with NFC Shiled V2.1

I try to use P2P_Push sample with NFC Shield V2.1 but failed. Regarding debug message, it seems fail to actiate PN532 Please let me know how to solve the problem? I already find a little bug and made issue on #82. But I can not fix the problem. The debug messaage on activate is as below. --- Send a ...
by dan295
Thu Jun 20, 2019 7:59 pm
Forum: Arduino & Seeeduino
Topic: mbed drive can not detect.
Replies: 4
Views: 852

Re: mbed drive can not detect.

I also checked on OSX and it still does not work.
Same behavior.
by dan295
Wed Jun 19, 2019 2:35 pm
Forum: Arduino & Seeeduino
Topic: mbed drive can not detect.
Replies: 4
Views: 852

Re: mbed drive can not detect.

Hi bill.yu

I connected the USB interface (next to 'BUTTON') of Arch Pro to your PC using a USB Micro B cable. But, it doesn't appears as a USB device named MBED.

Arch Pro is quiet new board. I bought it yesterday, and I just connect it once.
Only first time, the MBED drive appered.

Thanks.
by dan295
Tue Jun 18, 2019 11:48 am
Forum: Arduino & Seeeduino
Topic: mbed drive can not detect.
Replies: 4
Views: 852

mbed drive can not detect.

I use Arch Pro.
I connect it to Windows PC via Debug USB port with pressing Button, It can detect as "MBED LOADER" Drive.
But I connect it without pressing the button, it can not detect either "MBED LOADER" drive and "MBED" drive.

How to detect it as "MBED" Drive?
by dan295
Tue Apr 16, 2019 7:20 pm
Forum: Wio Series
Topic: Can I use WioLTE in France?
Replies: 1
Views: 597

Can I use WioLTE in France?

Can I use WioLTE in France with EU version? And, if I can, which career should I use in there?

I'm in Japan. So, I have not enought information about WioLTE information in France.
by dan295
Fri Jan 18, 2019 2:01 am
Forum: To Be Classified
Topic: Schematic of Wireless Charging Module
Replies: 3
Views: 1179

Re: Schematic of Wireless Charging Module

not yet
by dan295
Wed Jan 09, 2019 11:28 am
Forum: To Be Classified
Topic: Schematic of Wireless Charging Module
Replies: 3
Views: 1179

Schematic of Wireless Charging Module

Where can I get schematic of Wireless Charging Module - 5V 1A(SKU 106990017)

https://www.seeedstudio.com/Wireless-Ch ... -1912.html