Search found 4 matches

by davidpodless
Wed Jan 30, 2019 4:16 pm
Forum: ReSpeaker
Topic: Recording via python with Sample Rate over 16Khz
Replies: 2
Views: 975

Re: Recording via python with Sample Rate over 16Khz

Hi, I didn't received any answer regrading this issue. Can I record in higher rate than 16kHz in the ReSpeaker Mic Array v2.0? In your site you say the max rate is 48kHz but python send an error "OSError: [Errno -9997] Invalid sample rate" for the following rates: 44000, 44100, 48000. So, what is th...
by davidpodless
Mon Dec 10, 2018 7:02 pm
Forum: ReSpeaker
Topic: Source code of the DOA
Replies: 2
Views: 673

Re: Source code of the DOA

absolutely understandable
thank you for the reply
by davidpodless
Mon Dec 10, 2018 5:58 pm
Forum: ReSpeaker
Topic: Source code of the DOA
Replies: 2
Views: 673

Source code of the DOA

Hi, where can I the source code for the DOA of the ReSpeaker?
thank you
by davidpodless
Mon Dec 10, 2018 5:52 pm
Forum: ReSpeaker
Topic: Recording via python with Sample Rate over 16Khz
Replies: 2
Views: 975

Recording via python with Sample Rate over 16Khz

Hi,
In the specifications of v2, it says that the max sample rate of the ReSpeaker is 48Khz.
I tried to do it in python and it sent me an error.
What parameter should I send in order to record at 44 or 48Khz?
thanks