Search found 17 matches

by catherine12297
Wed Jan 09, 2019 4:40 pm
Forum: Fusion PCB/ PCBA Services
Topic: Some suggestions for parts in the OPL
Replies: 3
Views: 6853

Re: Some suggestions for parts in the OPL

The N-channel transistor that is accessible is just 20 V DS and 8 V GS. I'd like a little N-channel transistor with no less than 30 V DS and 20 V GS. This is helpful for: - Turn around extremity insurance on info. GS should be most extreme bolstered input voltage. - Reverse counteractive action afte...
by catherine12297
Mon Jan 07, 2019 6:24 pm
Forum: Fusion PCB/ PCBA Services
Topic: Drilling hole sizes -- what are the differences?
Replies: 2
Views: 2910

Re: Drilling hole sizes -- what are the differences?

0.3 vias accessible.
0.8 - littlest mounting gap, I think... mounting opening penetrating at last handling. they has not copper layer inside
by catherine12297
Sat Jan 05, 2019 4:15 pm
Forum: Fusion PCB/ PCBA Services
Topic: 4 layer DRU rules - min width 8 mil ?
Replies: 2
Views: 2451

Re: 4 layer DRU rules - min width 8 mil ?

6 mil would be the base and you are less inclined to have issues in the event that you use 8 mil. This is very basic with ease PCB providers - they incline toward somewhat bigger clearances than the base.
by catherine12297
Fri Jan 04, 2019 7:36 pm
Forum: Fusion PCB/ PCBA Services
Topic: Plated slot with G85 command
Replies: 2
Views: 5140

Re: Plated slot with G85 command

I would really like to know this too, I am about to send a file with G85 codes, but it breaks in the preview.
by catherine12297
Thu Jan 03, 2019 6:36 pm
Forum: Fusion PCB/ PCBA Services
Topic: what is the difference between PLC and SCADA.
Replies: 1
Views: 1262

what is the difference between PLC and SCADA.

I want to know about the difference between PLC and SCADA.
by catherine12297
Fri Dec 28, 2018 3:03 pm
Forum: Fusion PCB/ PCBA Services
Topic: Approving DRC errors okay?
Replies: 2
Views: 2801

Re: Approving DRC errors okay?

indeed, you can ingore it.
I recommend you can set the leeway of same flags as 0mil in DRC rule, the blunders will be vanished.
have a pleasant day!
dingding
by catherine12297
Wed Dec 26, 2018 6:16 pm
Forum: Fusion PCB/ PCBA Services
Topic: PNIODiag handling multiple PLC's
Replies: 0
Views: 916

PNIODiag handling multiple PLC's

PNIODiag handling multiple plc
by catherine12297
Tue Dec 25, 2018 3:27 pm
Forum: Fusion PCB/ PCBA Services
Topic: How to design PCB?
Replies: 1
Views: 1169

How to design PCB?

I want to know that how can we design PCB.
by catherine12297
Thu Dec 20, 2018 5:22 pm
Forum: Fusion PCB/ PCBA Services
Topic: Printed circuit board Assembly Process?
Replies: 0
Views: 1091

Printed circuit board Assembly Process?

Hell every one,

I want to know about the printed circuit board assembly process?
by catherine12297
Wed Dec 19, 2018 6:16 pm
Forum: Fusion PCB/ PCBA Services
Topic: Should pads & vias be included on the internal layers?
Replies: 2
Views: 3219

Re: Should pads & vias be included on the internal layers?

In a perfect world you ought to incorporate non-associated cushions on inner layers. It helps amid the plating procedure to have extra copper to plate to down the barrel of the opening. The annular rings don't need to be as enthusiastic about the inside layers as there are no tracks prompting them a...