Search found 145 matches

by schmron
Wed Jul 18, 2012 11:35 pm
Forum: To Be Classified
Topic: Seeedstudio has a spam problem
Replies: 1
Views: 2092

Re: Seeedstudio has a spam problem

This is my last post in this forum.

The spam problem here is terrible.
by schmron
Tue Jul 17, 2012 1:57 pm
Forum: Bee series & WSN
Topic: Multiple Bluetooth Bee Slaves?
Replies: 5
Views: 3744

Re: Multiple Bluetooth Bee Slaves?

seanl wrote: do you know any other board that's capable of multiple BT serial interfaces?

No.
I think you wouldn't find a device to use with 8-bit microcontroller.
by schmron
Tue Jul 17, 2012 10:12 am
Forum: To Be Classified
Topic: Seeedstudio has a spam problem
Replies: 1
Views: 2092

Seeedstudio has a spam problem

It's very hard to read this forum...
Why nobody delete the spam?!
by schmron
Tue Jul 17, 2012 10:08 am
Forum: Bee series & WSN
Topic: Multiple Bluetooth Bee Slaves?
Replies: 5
Views: 3744

Re: Multiple Bluetooth Bee Slaves?

However, right now I'm trying to combine both slaves into my project, so that the master will be able to communicate with two slaves at the same time This want work because the module can't create multiple serial interfaces like linux or windows. You can only pair with one device and have only one ...
by schmron
Tue Jul 17, 2012 9:54 am
Forum: Shields
Topic: arduino bluetooth shield + amarino
Replies: 4
Views: 3950

Re: arduino bluetooth shield + amarino

Hey! I'm trying to use the amarino library to simplify the communication between android tablet and arduino, but i'm stuck already at the first steps. i have this shield: http://www.seeedstudio.com/wiki/index.php?title=Bluetooth_Shield and arduino UNO. i tried uploading the sketch slave.pde to ardu...
by schmron
Tue Jul 17, 2012 9:44 am
Forum: Shields
Topic: Bluetooth Shield input scrambled
Replies: 3
Views: 2643

Re: Bluetooth Shield input scrambled

I'm having the same issue. Ubuntu 12.04, Arduino 1.01. I've tried switching to different TX/RX pins as suggested in other threads from people who have complained about this, with no luck. schmron, most of the things you brought up were the way they were in the example code for the product. Setting ...
by schmron
Fri Jul 13, 2012 11:28 am
Forum: Arduino & Seeeduino
Topic: Seeeduino mega v1.23 + arduino ethernet shield + IDE v1.0.1
Replies: 3
Views: 2777

Re: Seeeduino mega v1.23 + arduino ethernet shield + IDE v1.

I think the Ethernet Shield don't get a address from DHCP.
Try to use static IP. If it works, the problem isn't arduino but your DHCP server
by schmron
Fri Jul 13, 2012 11:14 am
Forum: Grove
Topic: info about the groove touch help needed....
Replies: 4
Views: 2768

Re: info about the groove touch help needed....

shazy792 wrote:Thanks for the info but i wanna know can i program this button for debounce and will it work stand alone
No its just a button. You need a circuit or microcontroller to use it
by schmron
Fri Jul 13, 2012 5:09 am
Forum: Grove
Topic: info about the groove touch help needed....
Replies: 4
Views: 2768

Re: info about the groove touch help needed....

Search for "Impulse relay" or "solid state relay" and "button debouncing".
Grove touch button is like a simple button.