Search found 5 matches
- Thu Sep 05, 2019 1:54 am
- Forum: Grove
- Topic: Grove Selection Guide - Feed-back
- Replies: 1
- Views: 978
Grove Selection Guide - Feed-back
Hi! Congratulations for the excellent initiative of the Grove Selection Guide! Actually, I've been maintaining my own list for a while. As some modules may require 5V for power but operate the I²C bus at 3.3V, may I suggest to mention two voltages: one for Signal Voltage, another for Power Voltage? ...
- Tue Aug 06, 2019 6:01 pm
- Forum: New Product Ideas
- Topic: NEW Releasing: STM32MP157C Development Board and Look forward to your ideas!
- Replies: 26
- Views: 10723
Re: NEW Releasing: STM32MP157C Development Board and Look forward to your ideas!
Hi!
This is a great initiative!
Which port the Grove connector provides? I hope I²C.
Which SDK (or SDKs) do you plan to use for the Cortex-M4 core? Apart from STM32Cube, do you plan to consider the Wiring/Arduino framework!
Good luck with the development!
This is a great initiative!
Which port the Grove connector provides? I hope I²C.
Which SDK (or SDKs) do you plan to use for the Cortex-M4 core? Apart from STM32Cube, do you plan to consider the Wiring/Arduino framework!
Good luck with the development!
- Fri Feb 22, 2019 7:27 pm
- Forum: Complaints and Suggestions
- Topic: Confusing Websites
- Replies: 1
- Views: 1657
Confusing Websites
There are currently two websites: https://www.seeedstudio.com https://www.seeedstudio.io This is very confusing. Are they both legit? When I tried to use the 40% off coupon ($20 off for any order over $50) on www.seeedstudio.io, some products were available but raised the error Quantity exceeds our ...
- Fri Feb 22, 2019 7:16 pm
- Forum: To Be Classified
- Topic: Pinout 125Khz RFID Module
- Replies: 2
- Views: 2562
Re: Pinout 125Khz RFID Module
Updating the wiki page with the correct pin-out would be great.
- Fri Feb 22, 2019 7:15 pm
- Forum: Azure Sphere Dev Kit
- Topic: Support for Cortex-M4Fs
- Replies: 2
- Views: 2304
Support for Cortex-M4Fs
According to the Azure Sphere MT3620 Development Kit product page, Please note that the current Azure Sphere software release does not support all features of the MT3620 hardware, including the two general purpose ARM Cortex-M4F cores, some peripheral interfaces (ADC, I2C, I2S, PWM and SPI), Wi-Fi 8...