Search found 7 matches
- Sat Aug 05, 2017 4:13 am
- Forum: DSO
- Topic: BenF 3.x FW on new LCD driver devices [flick. screen solved]
- Replies: 84
- Views: 126720
Re: BenF 3.x FW on new LCD driver devices [flick. screen sol
..... And...... initial attempt, using a Linux machine (UBUNTU 16.04/AMD 64X2/8GB Mem), FAILED... no change, it still had the blank-white screen.. However......... I think I went to the MIN main forum, and located a post, that had two .hex files, claiming to be the original firmware... tried it via ...
- Thu Jul 27, 2017 2:25 am
- Forum: DSO
- Topic: BenF 3.x FW on new LCD driver devices [flick. screen solved]
- Replies: 84
- Views: 126720
Re: BenF 3.x FW on new LCD driver devices [flick. screen sol
Not yet.. Just downloaded it today, (still cleaning out my email box.) will let you know if it worked, or not..
- Wed May 17, 2017 7:19 pm
- Forum: DSO
- Topic: BenF 3.x FW on new LCD driver devices [flick. screen solved]
- Replies: 84
- Views: 126720
Re: BenF 3.x FW on new LCD driver devices [flick. screen sol
Rimidalv007, the file LIB301_APP311_2.ZIP doesn't appear to be active anymore (unable to deliver file).. anywhere else I should be looking? I'm still sitting here with a brick. (Serial B5DDCA09 License F6E6698C) (Yes, I got it from Ebay)... Unfortunately, it choked on BenF 3.45D. Neither is Motorpas...
- Wed Feb 01, 2017 2:42 am
- Forum: DSO
- Topic: BenF 3.x FW on new LCD driver devices [flick. screen solved]
- Replies: 84
- Views: 126720
Re: BenF 3.x FW on new LCD driver devices [flick. screen sol
Do either the V2 or V3 files exist? When I try to download them, it reports file cannot be transferred.. Still stuck with a brick... 

- Fri Jan 27, 2017 9:59 am
- Forum: DSO
- Topic: DSO nano new bootloader firmware
- Replies: 120
- Views: 156429
Re: DSO nano new bootloader firmware
I think I hit the same problem.. copied the BenF .hex files to my 201, and it bricked to a white/grey screen.. It also produced a .err file when it remounted... (pretty sure it was BenF 4.6.2 -App that bricked it.) Obtained the rar file from the link someone else provided. Hope it fixes things, Othe...
- Sun May 08, 2011 9:27 pm
- Forum: To Be Classified
- Topic: Can't upgrade to BenF's code
- Replies: 3
- Views: 3336
Re: Can't upgrade to BenF's code
I think I've hit another oddity.. Though I may also know why.. Is there a limit to the number of times you can use DfuSE Demo? I have been trying different firmwares on my DSO, and yesterday, the DfuSE demo program refused to start. So, presently I'm locked into E-Design's 2.31. (and I want to put B...
- Thu Apr 21, 2011 2:19 pm
- Forum: DSO
- Topic: Unable to save to card
- Replies: 5
- Views: 5182
Re: Unable to save to card
I seem to have run into this problem too.. I bought mine through a seller in New York, Via eBay. the card is a PNY 2GB Micro-SD, bought at the local Staples store.. It would appear, some of these may have a bad SD card slot.. Presently running BenF's 3.61 firmware. I also get the "SD Err" error.. Or...