yes, you can connect both of sensors to the node.
you can connect the moisture sensor to J8 , this is a analog port, and connect the temprature&humidy sensor to J9 , this is a digital port , it will works fine.
thanks
Search found 232 matches
- Fri Aug 02, 2013 3:24 pm
- Forum: Grove
- Topic: Wireles Sensr Node + 2 Nodes = How To ?
- Replies: 1
- Views: 1821
- Fri Jul 26, 2013 11:49 am
- Forum: Fusion PCB/ PCBA Services
- Topic: Questions from Propagate Newbie
- Replies: 2
- Views: 2282
Re: Questions from Propagate Newbie
1. For the first round of production, do you still provide components out of your component pool? Yes, we can help you sourcing you required components. and if you use the components in the OPL, this work would be much easier. 2. Which components in your Components pool are free? Do you have rough ...
- Tue Jul 02, 2013 10:09 am
- Forum: Grove
- Topic: Grove - Sound Recorder - SEN71254P
- Replies: 1
- Views: 1627
Re: Grove - Sound Recorder - SEN71254P
hi , actually, the sound recorder do not has a library, you can control the module by pressing the button or by serial command. please refer to the http://www.seeedstudio.com/wiki/Grove_- ... rder#Usage to get the step-by-step guidance.
thanks .
thanks .
- Mon Jun 03, 2013 10:01 am
- Forum: To Be Classified
- Topic: Check update firmware
- Replies: 4
- Views: 3972
Re: Check update firmware
er....
a bit confused, i think their is no firmware for the lipo rider pro....

a bit confused, i think their is no firmware for the lipo rider pro....
- Mon Jun 03, 2013 9:52 am
- Forum: Arduino & Seeeduino
- Topic: Power jack size for Rainbowduino v3.0
- Replies: 3
- Views: 2511
- Sun Apr 28, 2013 3:33 pm
- Forum: Grove
- Topic: Circular LED on Mega?
- Replies: 7
- Views: 5906
Re: Circular LED on Mega?
it is not i2c, you can download library source code in the wiki for reference. ...
- Tue Apr 02, 2013 1:55 pm
- Forum: Grove
- Topic: Grove XBee Carrier - RESET
- Replies: 5
- Views: 3739
Re: Grove XBee Carrier - RESET
this button really confusing sometimes. 

- Fri Mar 29, 2013 4:08 pm
- Forum: Shields
- Topic: Bluetooth Shield on Arduino due
- Replies: 2
- Views: 1858
Re: Bluetooth Shield on Arduino due
hi, as the bluetooth shield communicate with MCU board(Uno or Due) by uart. so, you just need to use the UART port to receive or sent message via the Bluetooth. the Bluetooth is compatible with Uno to Due by Hardware. but note that you need to set the serial port in Due.
- Tue Mar 19, 2013 11:40 am
- Forum: Grove
- Topic: problem with codec-adaptive wireless relay
- Replies: 4
- Views: 2824
Re: problem with codec-adaptive wireless relay
hi, sir , the enable pin need pulse rising edge to enable the setting, so , you need to first digitalwrite low to the enable , and then digitalwrite HIGH to this pin. for example: void turnSwitchOnOff(byte sw) { digitalWrite(sw,HIGH); // set the relay state. /// gives a rising edge to enable pin dig...
- Fri Mar 01, 2013 5:17 pm
- Forum: Grove
- Topic: Grove - Circular LED
- Replies: 3
- Views: 1432
Re: Grove - Circular LED
have a try of this.....good luck...