Search found 65 matches

by salmanfarisvp
Thu Dec 12, 2019 4:57 pm
Forum: Shields
Topic: SeeedStudio TFT Touch Shield 2.8" v2.1 with D1 R32 ESP32 (ESPDUINO-32)
Replies: 1
Views: 608

Re: SeeedStudio TFT Touch Shield 2.8" v2.1 with D1 R32 ESP32 (ESPDUINO-32)

hi ,

Did you try the SeeedStudios TFTv2 lib? Please let me know the output
by salmanfarisvp
Thu Dec 12, 2019 4:55 pm
Forum: Grove
Topic: Firmware for Grove Triple Color E-Ink Display 2.13"?
Replies: 1
Views: 283

Re: Firmware for Grove Triple Color E-Ink Display 2.13"?

hi ,

Are you looking for the source code for the programme? check this: https://github.com/Seeed-Studio/Grove_T ... de_213.ino
by salmanfarisvp
Thu Dec 12, 2019 4:52 pm
Forum: Grove
Topic: Enclosure for the Grove - CO2 & Temperature & Humidity Sensor (SCD30)
Replies: 1
Views: 143

Re: Enclosure for the Grove - CO2 & Temperature & Humidity Sensor (SCD30)

Hi ,

What kind of matrial are you looking for ? Do you need customized or readymade box will help you ?
by salmanfarisvp
Wed Dec 11, 2019 11:08 pm
Forum: ReSpeaker
Topic: Deep Learning on Respeaker Core V2
Replies: 1
Views: 847

Re: Deep Learning on Respeaker Core V2

Hi,
Since the Respeker Core V2 is GNU/Linux based operating system you can run the tensorflow or pytorch implementations . you can take the example with honk , honk is a PyTorch implementations of neural network models for keyword spotting http://honk.ai/ .
by salmanfarisvp
Tue Dec 10, 2019 1:37 pm
Forum: Grove
Topic: Help to understand what Grove is
Replies: 1
Views: 76

Re: Help to understand what Grove is

Hi , Grove Zero is a STEM Starter Kit , which is a set of colour-coded and magnetic electronic modules that teaches students about programming, electronics, design thinking, and logics. The Grove Zero modules are designed for STEM education and it allows teachers with no experience or lots of experi...
by salmanfarisvp
Mon Dec 09, 2019 2:22 pm
Forum: Grove
Topic: Grove for microbit, increase software package with newer sensors
Replies: 3
Views: 101

Re: Grove for microbit, increase software package with newer sensors

Hi,

What problem you are facing while working with barometer sensor (BMP280) and 4 digit display? Can you please elaborate the issues.
by salmanfarisvp
Mon Dec 09, 2019 2:18 pm
Forum: Grove
Topic: Grove - Finger-clip Heart Rate Sensor
Replies: 1
Views: 33

Re: Grove - Finger-clip Heart Rate Sensor

Hi Tsl.

Yes, you can use, since the Grove - Finger-clip Heart Rate Sensor is using I2C interface you can connect with the micro:bit I2C Interface.

Grove - Finger-clip Heart Rate Senso WiKi :http://wiki.seeedstudio.com/Grove-Finge ... te_Sensor/
by salmanfarisvp
Mon Dec 09, 2019 1:31 pm
Forum: Shields
Topic: Relay Shield v3.0 Power Supply
Replies: 3
Views: 86

Re: Relay Shield v3.0 Power Supply

You can use the VIN pin , VIN is the completely unaltered input power before the regulator.
by salmanfarisvp
Sat Dec 07, 2019 3:02 pm
Forum: Arduino & Seeeduino
Topic: Seeeduino with Grove
Replies: 2
Views: 105

Re: Seeeduino with Grove

Hi, here is the code for reading the Soil Moisture. int sensorPin = A0; int sensorValue = 0; void setup() { Serial.begin(9600); } void loop() { // read the value from the sensor: sensorValue = analogRead(sensorPin); Serial.print("Moisture = " ); Serial.println(sensorValue); delay(1000); } Here we ar...