Search found 17 matches

by bluedude
Sun Nov 17, 2013 11:37 pm
Forum: Bee series & WSN
Topic: WIFI bee 2.0, WSN as standalone sensor node
Replies: 1
Views: 2183

WIFI bee 2.0, WSN as standalone sensor node

Can the WIFI 2.0 Bee be used with the Wireless Sensor Node stuff to create a wireless node that can send sensor data through the WIFI connection?

If yes, any samples?

Cheers,
by bluedude
Tue Sep 10, 2013 1:11 am
Forum: Grove
Topic: Grove enclosures
Replies: 1
Views: 1623

Grove enclosures

Hi,

I'm a big fan of Grove and now you introduced Grove Mixr but it makes me wondering. Why didn't you create the same nice enclosures for Grove modules first?

There is no good enclosure system for Grove modules. Instead you created another product line, kind of disappointing.

Cheers,
by bluedude
Sun Mar 10, 2013 12:14 am
Forum: Grove
Topic: Grove connectors on cables
Replies: 1
Views: 1696

Grove connectors on cables

Where can I get JST connectors that are the same as the ones on the Grove cables? I want to create my own longer cables.

Is there equipment to do this?

What is the exact type and model of these connectors?

Could I easily add these connectors to other types of sensors?

Cheers
by bluedude
Mon Oct 01, 2012 2:20 pm
Forum: Bee series & WSN
Topic: RFBee firmware configuration
Replies: 2
Views: 4062

RFBee firmware configuration

How can I change configuration parameters to set the radio in 868 mode? For now I have set some parameters in the reset but that isn't the best way. Should it be in Config.h? / config layout #define CONFIG_RFBEE_MARKER 0 // Marker #define CONFIG_HW_VERSION 1 // Hardware version #define CONFIG_FW_VER...
by bluedude
Fri Sep 28, 2012 9:41 pm
Forum: Bee series & WSN
Topic: RFBee, Arduino WirelessProtoShield and standalone carrier
Replies: 0
Views: 1708

RFBee, Arduino WirelessProtoShield and standalone carrier

Hi, Can anyone help to get the following done: - have some code for an Arduino + Wireless Proto Shield + RF Bee functioning as a wireless sensor base station; - have some code for the standalone node (Firmware 1.1 works) to send to the base station. I have no clue how to use the RFBee with the Wirel...
by bluedude
Thu Sep 27, 2012 10:48 pm
Forum: Grove
Topic: Sten carrier, solar kit and two RFBees
Replies: 0
Views: 1633

Sten carrier, solar kit and two RFBees

Hi, I want to create a base station with one RFBee attached to an Arduino and a remote node that uses and RFBee with the Stem carrier. How do I need to program these to do this? Which board should I select to program them? Till now nothing actually works. Has anyone done this before (which seems to ...
by bluedude
Mon Sep 03, 2012 6:19 pm
Forum: Grove
Topic: Grove LED with jumper cables
Replies: 1
Views: 1694

Grove LED with jumper cables

Hi,

I want to hookup a Grove LED to an Arduino without using a base shield. Which of the wires (red, white, black and yellow) should I connect to which pin?

Cheers,
by bluedude
Fri Apr 06, 2012 4:17 pm
Forum: Grove
Topic: Dragrove and CE certification
Replies: 3
Views: 2633

Re: Dragrove and CE certification

Did you replace the original board that has certification or did you add something?

Cheers,
by bluedude
Fri Apr 06, 2012 2:27 am
Forum: Grove
Topic: Is support staff actually answering questions in here?
Replies: 5
Views: 3354

Re: Is support staff actually answering questions in here?

Tried that too :-(

It is a shame that a company with such interesting products lacks major in documentation (certified components for Europe), support and pre-sales.

Very disappointed.
by bluedude
Wed Apr 04, 2012 4:28 pm
Forum: Grove
Topic: Is support staff actually answering questions in here?
Replies: 5
Views: 3354

Is support staff actually answering questions in here?

Hi,

Is anyone of the support staff actually answering questions in here?

Cheers,