Search found 2 matches

by ricardo.herrero
Wed Oct 02, 2019 2:26 pm
Forum: Shields
Topic: need information about solar charger shield V2.2
Replies: 4
Views: 1032

Re: need information about solar charger shield V2.2

I have seen three different connectors but I can´t decide which one is the proper one:
JST PH 2 pin
JST XH 2 pin
JST XHP-2

Which should I choose? This is info that should come with the solar charger v2.2 shield.

Thanks for the help!
Ricardo
by ricardo.herrero
Mon Sep 30, 2019 7:24 pm
Forum: Shields
Topic: need information about solar charger shield V2.2
Replies: 4
Views: 1032

Re: need information about solar charger shield V2.2

Hello, Thanks for the info, I have seen this answer and I will buy the cables, but I also need the connector. I have seen both 2.00mm and 2.54mm. I have bought solar charger v2.2 11/19/2014, which one is valid for me? From the wikipedia we can see the type of connector, which one do I choose? Thanks...