Search found 735 matches

by bill.yu
Mon Nov 11, 2019 5:47 pm
Forum: Grove
Topic: Connection confusion
Replies: 2
Views: 367

Re: Connection confusion

Hello, Different interfaces on Base Shield use the other 2 pins for different purpose. For example, 4 pins of UART are GND, VCC, TX, RX, while TX and RX are used for data transmitting and receiving. By modifying pins configuration in the source code you can determine what pin you want to use. BTW, d...
by bill.yu
Fri Nov 01, 2019 5:51 pm
Forum: Grove
Topic: Grove GPS with Grove Base Hat for Raspberry Pi (Changing port definitions?)
Replies: 3
Views: 596

Re: Grove GPS with Grove Base Hat for Raspberry Pi

Hi there~

It's compatible but you need to modify source code to change the port.
by bill.yu
Fri Oct 18, 2019 3:20 pm
Forum: Grove
Topic: Is there a Grove connector eInk display?
Replies: 3
Views: 575

Re: Is there a Grove connector eInk display?

Here is the link to 2.7'' Triple-Color E-Ink Shield for Arduino:

https://www.seeedstudio.com/2-7-Triple- ... -4069.html
by bill.yu
Mon Oct 14, 2019 5:16 pm
Forum: Grove
Topic: Is there a Grove connector eInk display?
Replies: 3
Views: 575

Re: Is there a Grove connector eInk display?

Hi there~

Yes, it is. It can be connected to port UART of Grove-Base Shield and we also have another Triple Color E-Ink Display whose dimension is 1.54''.

Here is the link:

https://www.seeedstudio.com/Grove-Tripl ... -2890.html

Thanks
best rgds
Jiangli
by bill.yu
Mon Sep 30, 2019 1:57 pm
Forum: Grove
Topic: control Grove RGB LED Ring and Seeeduino V4.2 under Matlab
Replies: 1
Views: 351

Re: control Grove RGB LED Ring and Seeeduino V4.2 under Matlab

Hi there~

In theory it's possible to control Grove RGB LED Ring and Seeeduino V4.2 under MATLAB but I'm so sorry we don't have such code.

Thanks sincerely,
JL
by bill.yu
Fri Sep 27, 2019 6:13 pm
Forum: Arduino & Seeeduino
Topic: Current draw of the Bluetooth Bee Standalone
Replies: 1
Views: 789

Re: Current draw of the Bluetooth Bee Standalone

Hi there~ We only have the schematic and the PCB. https://raw.githubusercontent.com/SeeedDocument/forum_doc/master/image/bluetooth-bee/PCB.PNG https://raw.githubusercontent.com/SeeedDocument/forum_doc/master/image/bluetooth-bee/schematic.PNG If you have any other questions, please give feedback to u...
by bill.yu
Fri Sep 27, 2019 5:43 pm
Forum: Arduino & Seeeduino
Topic: XBEE SLEEP_RQ and CTS signals on Stalker V3.1
Replies: 1
Views: 653

Re: XBEE SLEEP_RQ and CTS signals on Stalker V3.1

Hi Todd According to documents, If you enable hardware flow control (D7 command), the CTS pin asserts (low) when the device wakes. There are two figures. Figure 1 shows where the CTS port is, and figure 2 shows the schematic of Stalker. You can see it's not connected to ATmega328P MCU. You need a ju...
by bill.yu
Fri Sep 27, 2019 3:45 pm
Forum: Grove
Topic: Voltaje divider supply
Replies: 3
Views: 522

Re: Voltaje divider supply

Hello Are you using Arduino board to build your sensor? If you're using it, normally the working voltage of Arduino is 5V, and you can connect your battery directly to analog port (The max output voltage of Lipo battery is 3.7V), and if your working voltage of Arduino is 3.3V, you can use two 1k res...
by bill.yu
Fri Sep 27, 2019 10:39 am
Forum: Hardware Products for AIoT Applications
Topic: Sipeed Support
Replies: 0
Views: 1586

Sipeed Support

Hi there~,

For Sipeed support, please post questions to https://bbs.sipeed.com/ or drop mail to support@sipeed.com. thanks.
by bill.yu
Fri Sep 27, 2019 10:34 am
Forum: Raspberry Pi
Topic: Raspberry Pi HeatSink
Replies: 5
Views: 1241

Re: Raspberry Pi HeatSink

Hi there~

We will release the case soon. Please stay tuned. thanks.