Search found 5 matches

by ivanlomy
Fri Apr 20, 2018 9:41 pm
Forum: Grove
Topic: HCHO sensor data intepretation help
Replies: 3
Views: 4271

Re: HCHO sensor data intepretation help

I found this sample code, may be this is correct, I dun know.

https://www.himix.lt/arduino/arduino-an ... ol-sensor/

I hope the Seeedstudio engineer can verify this code, or provide some easy understanding code for us here. The HCHO sensor wiki is really confusing.

Thx
by ivanlomy
Tue Apr 17, 2018 10:26 pm
Forum: Arduino
Topic: Seeeduino and Seeeduino Cloud USB power bank
Replies: 1
Views: 633

Seeeduino and Seeeduino Cloud USB power bank

Really love to power up my Seeeduino and Seeeduino Cloud by portable PowerBank. The spec of my USB PowerBank is: 10000mAh 3.85V ( 38.5Wh ) input 5.0V2.0A 9V/12V18W output 5.1V2.0A 9V/12V12W for this spec, it is safe to power up my boards? for long operation hrs (1 months) also safe? If I use other P...
by ivanlomy
Fri Apr 13, 2018 9:34 pm
Forum: Arduino
Topic: Seeeduino Cloud works with Thinger.io?
Replies: 0
Views: 519

Seeeduino Cloud works with Thinger.io?

I am newbie, I try to run an thinger.io example code with my Seeeduino Cloud, but no luck. I did setup an account at thinger.io and added device id and its credential. Also I checked the seeeduino cloud is able to access internet (run httpclicent example b4) Is the seeeduino support thinger.io sdk? ...
by ivanlomy
Thu Apr 12, 2018 12:46 am
Forum: Grove
Topic: Grove Infrared Emitter doest work on Seeeduino Cloud
Replies: 2
Views: 783

Re: Grove Infrared Emitter doest work on Seeeduino Cloud

Jelly, you really save my day.... BIG THANK YOU I followed your method without the base shield, it works perfectly. However, I tried your method with base shield, it still works perfectly... If I use it like this with base shield, is everything fine? safe without blow it up? Because I really want to...
by ivanlomy
Wed Mar 28, 2018 7:01 pm
Forum: Grove
Topic: Grove Infrared Emitter doest work on Seeeduino Cloud
Replies: 2
Views: 783

Grove Infrared Emitter doest work on Seeeduino Cloud

I run the example code IRSendRev (send) ( https://github.com/Seeed-Studio/IRSendRev ) on both Seeeduino Cloud and Seeeduino boards, each boards is attached by Base Shield V2 and the Grove IR-Emitter is set on D3. The Seeeduino is running fine and IR signal emitted perfectly, but the Seeeduino Cloud ...