Search found 4 matches

by southernblackdragon
Sat Apr 16, 2011 2:26 am
Forum: DSO
Topic: Which firmware can I use?
Replies: 11
Views: 7975

Re: Which firmware can I use?

I too bought a DSO Nano off ebay from a hongkong based seller, reached pretty quickly. This was also advertised as v1.6 of the hardware revision and apparently is supposed to be capable of 2Msps with a firmware update from the Paul's v1.5 F/W that it is shipped with. I switched to BenF v3.61 on day...
by southernblackdragon
Sat Apr 09, 2011 12:45 am
Forum: DSO
Topic: DSO firmware version 3.64
Replies: 181
Views: 239478

Re: DSO firmware version 3.61

ingra- how would he do the ranges- there are 3 common ranges 1mv=1amp 10mv=1amp =100mv=1amp, it wouldnt be usefull unless all three were implimented, i use the first one for starter relitive compression checks, the second one for alternator ripple measurements and diesel injectors.. and the third i...
by southernblackdragon
Tue Aug 03, 2010 11:07 am
Forum: DSO
Topic: Can't install Dfuse driver on windows xp spanish
Replies: 2
Views: 3002

Can't install Dfuse driver on windows xp spanish

Hello, sorry for my bad english, I wonder if someone could help me install Dfuse On windows xp spanish language. Every time i try to install it i get a message in spanish kind of like this "the driver manger does not support the language, contact your program provider" I want to install Paul's firmw...
by southernblackdragon
Thu May 06, 2010 2:43 am
Forum: DSO
Topic: Can Non-invasive AC current sensor work with the NANO
Replies: 1
Views: 2291

Can Non-invasive AC current sensor work with the NANO

hello, can someone tell me please if an ac current sensor, like the one seeedstudio offers (Model: SCT-013-030), work with the dso nano?, I'am asking this because, I want to measure 12v solenoids (like the fuel injectors found in a car),with less than 30A . Also I'am planning to use my DSO Nano as a...