Search found 34 matches

by seth.welday
Thu Jul 11, 2019 4:44 pm
Forum: ReSpeaker
Topic: Voice Activity Detection (VAD) on ReSpeaker_4-Mic_Linear_Array
Replies: 3
Views: 1867

Re: Voice Activity Detection (VAD) on ReSpeaker_4-Mic_Linear_Array

A bit late to the party. The XMOS chip can work with a linear array, but it would have to be designed an laid out. Seeed can provide this service if you commit to ordering and paying for the customization. Essentially we have a minimal price for this kind of service. If you want to know more you can...
by seth.welday
Thu Apr 25, 2019 11:48 am
Forum: New Product Ideas
Topic: NEW Product Idea:Grove Kit compatible with NVIDIA Jetson Nano
Replies: 11
Views: 95932

Re: NEW Product Idea:Grove Kit for NVIDIA Jetson Nano

It would be good to have a camera that could provide high frame rates with MIPI CSI-2. For machine vision high frame rates would be ideal. Not sure if this is possible through grove system. I don't think Grove could do this. Grove only has 4 pins, so that is GND, VCC, SDA, SCL (power and camera con...
by seth.welday
Mon Apr 22, 2019 11:26 am
Forum: Hardware Products for AIoT Applications
Topic: MAix GO/Dock/BiT Project Source Files
Replies: 3
Views: 1980

Re: MAix GO/Dock/BiT Project Source Files

Hey Amigo, I'm sending this thread over to our 3rd party product managers. I just want you to know your feedback (first post) will be seen by them. As for your question on better dimensions, I agree that mounting hole spacing should be on there... I'm going to ask the team to reach out to Sipeed for...
by seth.welday
Tue Apr 09, 2019 11:15 am
Forum: ReSpeaker
Topic: ReSpeaker Mic Array V2 and JAVA
Replies: 6
Views: 1601

Re: ReSpeaker Mic Array V2 and JAVA

Awesome! I'll ask our team to share it in the next couple of days. If I have the courage, I will write a small Java library for the Mic Array with a observable / listener system to send events when the data change, and I will add the "write" method. Don't be afraid to give it a shot. Developers in o...
by seth.welday
Mon Apr 08, 2019 2:59 pm
Forum: To Be Classified
Topic: Anti-spam measures
Replies: 17
Views: 39224

Re: Anti-spam measures

I saw your posts today. I will make sure the tech support team sees them as well.
by seth.welday
Mon Apr 08, 2019 11:14 am
Forum: w600 Module and Development Boards
Topic: What makes this different from ESP8266?
Replies: 3
Views: 3206

Re: What makes this different from ESP8266?

Yes. And we will have a:FreeRTOS, so it will easily integrate with some AWS services.
by seth.welday
Mon Apr 08, 2019 10:48 am
Forum: ReSpeaker
Topic: 2-mic and 4-mic linear array GPIO pins
Replies: 3
Views: 1458

Re: 2-mic and 4-mic linear array GPIO pins

I just thought I'd list the apparently unconnected GPIO pins in case anyone else has the same problem. Thanks! My question is really though, what's the intended method to access these unused (if they really are) GPIO pins? Soooooo..... yeah. This can be a bit difficult. If you want to use multiple ...
by seth.welday
Mon Apr 08, 2019 10:23 am
Forum: ReSpeaker
Topic: Raspi Pi w Camera NOIR - stopped working
Replies: 2
Views: 582

Re: Raspi Pi w Camera NOIR - stopped working

The bane of hardware development - a loose cable. I once spent an entire day uploading firmware onto 200 boards. Then I spent an additional day trying to figure out why the last two dev boards would not flash the firmware. Turns out I had used that specific USB cable so much the data lines had erode...
by seth.welday
Mon Apr 08, 2019 10:16 am
Forum: ReSpeaker
Topic: ReSpeaker Mic Array V2 and JAVA
Replies: 6
Views: 1601

Re: ReSpeaker Mic Array V2 and JAVA

Wow, this is great Nicolas! Glad to see you got this working.

Mind if we share this on social media? :D
Would love to show off your work!
by seth.welday
Fri Dec 28, 2018 2:49 pm
Forum: To Be Classified
Topic: Anti-spam measures
Replies: 17
Views: 39224

Re: Anti-spam measures

Hey Baqwas,

I made sure the administrators have seen this.

Cheers.