Search found 8 matches
- Mon Sep 09, 2019 7:05 pm
- Forum: Wio Series
- Topic: Wio Lite MG126 - errors when compiling
- Replies: 5
- Views: 823
Re: Wio Lite MG126 - errors when compiling
do I need to do this even when not using the bluetooth library?
- Mon Sep 09, 2019 7:04 pm
- Forum: Wio Series
- Topic: Wio Lite W600
- Replies: 5
- Views: 1137
Re: Wio Lite W600
The lost connection after a reset maybe related to the usb driver, idk. The other issue; any sketch using the W600 library fails to compile. For example, none of the examples will compile. Arduino: 1.8.9 (Windows 8.1), Board: "Seeeduino Wio Lite W600" WARNING: library Wire claims to run on (samd) ar...
- Sun Sep 08, 2019 3:28 pm
- Forum: Wio Series
- Topic: Wio Lite W600
- Replies: 5
- Views: 1137
Wio Lite W600
Hi, re-downloaded the Arduiono IDE board addon. Still no usb driver Seeeduino_SAMD_zero => 1.0.0 Currently using the usb driver you emailed to me. When uploading from the Arduino IDE the cpu resets. After the reset the board does not reconnect to the IDE. To get it to reconnect I have to manually re...
- Sun Sep 08, 2019 2:51 pm
- Forum: Wio Series
- Topic: Wio Lite MG126 - errors when compiling
- Replies: 5
- Views: 823
Wio Lite MG126 - errors when compiling
Hi, I have a fresh install of Arduino 189, downloaded the Wio Lite MG126 boards addon. I am getting the following error when trying to compile basic sketches (even empty sketches): Tried the button example, the get_bat_val example and many very small basic sketches. Here is the normal error report f...
- Wed Aug 28, 2019 12:00 pm
- Forum: w600 Module and Development Boards
- Topic: Will the module support Arduino? Where can I find the SDK?
- Replies: 3
- Views: 1561
Re: Will the module support Arduino? Where can I find the SDK?
Hi,
is this still being developed? The last commit on github was Jan30th.
is this still being developed? The last commit on github was Jan30th.
- Wed Aug 28, 2019 11:55 am
- Forum: Wio Series
- Topic: Wio Lite W600. Windows 8.1 driver
- Replies: 0
- Views: 549
Wio Lite W600. Windows 8.1 driver
Hi, I am having problems finding a Windows driver for the Wio Lite W600 and Wio Lite MG126. Windows 8.1 (home) Windows Update Driver Software does not find anything. Seeeduino_SAMD_zero V1.0.0 Seeeduino_WioLite_MG126 v1.0.0 The boards definitions do not include drivers.I have tried alternative drive...
- Tue Aug 27, 2019 12:55 pm
- Forum: w600 Module and Development Boards
- Topic: Will the module support Arduino? Where can I find the SDK?
- Replies: 3
- Views: 1561
Re: Will the module support Arduino? Where can I find the SDK?
It looks like there has been no new activity on the Arduino SDK since Jan 30, Are you still developing the Arduino SDK?
- Mon Aug 26, 2019 7:12 pm
- Forum: w600 Module and Development Boards
- Topic: Wio Lite W600 USB Driver for Windows?J
- Replies: 2
- Views: 2529
Re: Wio Lite W600 USB Driver for Windows?J
I'm also having issues with a driver. Windows 8.1. Using an admin account on Windows, have installed the board addon and the driver was not installed. The device shows up in Device Manager but I get an error when I try to install the included driver manually. I also installed the Arduino Zero board ...