Search found 5 matches

by KvD
Sat Jan 30, 2010 8:48 pm
Forum: DSO
Topic: New firmware :DS0201_V2.2X
Replies: 37
Views: 28231

Re: New firmware :DS0201_V2.2X

Hi @all! @DETN8R: http://en.wikipedia.org/wiki/Jtag in short: JTAG is a direct connection to the processor, for debugging, monitoring, programming... If anything goes wrong while flashing the backup file i posted (power loss,...) or it´s simply not compatible to your hardware revision (i think it wo...
by KvD
Fri Jan 29, 2010 6:36 pm
Forum: DSO
Topic: New firmware :DS0201_V2.2X
Replies: 37
Views: 28231

Re: New firmware :DS0201_V2.2X

Hi. attached is a full backup of my original firmware. But be carefull, it rewrites the bootloader/update thing also. for me it works, but i can not guarantee that it works for you too. If anything goes wrong your DSO Nano could die and the only way to bring it back to life then is JTAG. USE IT AT Y...
by KvD
Fri Jan 29, 2010 8:26 am
Forum: DSO
Topic: mic input?
Replies: 1
Views: 2430

Re: mic input?

Hi.

no, there is no microphone integrated. the case was made for audio/video players and therefor the mic hole was...

cu.
by KvD
Sat Jan 16, 2010 7:03 am
Forum: DSO
Topic: How to load new firmware into DSOnano?
Replies: 6
Views: 5319

Re: How to load new firmware into DSOnano?

Hi, again ;)

if the "eDesign DSO Flash Disk USB Device" is shown, the right driver is installed!

switch off your dso. press and hold the down button while switching on your dso to start in upgrade mode.

then start DfuSe. Now you should see your device...

hope it work for you...


cu.
by KvD
Sat Jan 16, 2010 5:30 am
Forum: DSO
Topic: How to load new firmware into DSOnano?
Replies: 6
Views: 5319

Re: How to load new firmware into DSOnano?

Hi. You can use DfuSe. As target select internal flash. With "Upload Action" you can choose a file and make a backup of your original firmware. And i think it´s important to do so before you flash a new firmware, so that you can go back to your original! With "Upgrade or Verify Action" you can flash...