Search found 23 matches

by pizzic
Mon Aug 27, 2018 11:33 pm
Forum: ReSpeaker
Topic: Mic array in UBUNTU
Replies: 4
Views: 1464

Re: Mic array in UBUNTU

Thank you Bill.

I tried with the firmware and audacity, and I get the same result. I need to try with the python script. I need some day to do it, because I do not have access to the mic now.
I'll let you know the result.
Thanks,
by pizzic
Fri Aug 24, 2018 11:06 pm
Forum: ReSpeaker
Topic: Mic array in UBUNTU
Replies: 4
Views: 1464

Re: Mic array in UBUNTU

Hello.
It's V1.
I'm attaching an MP3 recorded with audacity (also with other tools I have the same result). You can hear my voice in background saying "hello", but it's very distorted.
Thanks a lot for your help.
by pizzic
Thu Aug 23, 2018 11:42 pm
Forum: ReSpeaker
Topic: Mic array in UBUNTU
Replies: 4
Views: 1464

Mic array in UBUNTU

Hello.
I'm trying to use the ReSpeaker MIC array as USB MIC in Ubuntu. The MIC is recognized, but when I try to record something (with audacity for example), I just get a lot of background noise, and my voice is barely audible in the background.
Any suggestion to fix this?
Thanks,
by pizzic
Sat Dec 19, 2015 8:47 pm
Forum: Wearables
Topic: Xadow upload sketch
Replies: 4
Views: 4156

Re: Xadow upload sketch

OK, SOLVED:

I had to remove Modem Manager

#apt-get remove modemmanager

As a reference, see also

http://labs.arduino.org/Arduino+IDE+on+Linux-based+OS

thanks
by pizzic
Sat Dec 19, 2015 7:56 pm
Forum: Wearables
Topic: Xadow upload sketch
Replies: 4
Views: 4156

Re: Xadow upload sketch

Also, consider that I'm able to upload on different boards and on the old Xadow with the same IDE.
by pizzic
Sat Dec 19, 2015 6:21 pm
Forum: Wearables
Topic: Xadow upload sketch
Replies: 4
Views: 4156

Re: Xadow upload sketch

Thanks kavi.

Yes, I'm using Linux.

My user is already in the dialout group.

But now, which board should I use to upload? Leonardo or Xadow?

Thanks,
by pizzic
Mon Dec 14, 2015 2:07 am
Forum: Wearables
Topic: Xadow upload sketch
Replies: 4
Views: 4156

Xadow upload sketch

Hello. Some months ago I bought some Xadow main board. I was able to upload sketches with Arduino 1.5 by following the instructions given in the Wiki. So far so good. Recently I bought a couple of new main boards, but there is something strange: the board has now a different ID. It is recognized as ...
by pizzic
Wed Sep 23, 2015 4:57 am
Forum: Wearables
Topic: Xadow sleep mode
Replies: 2
Views: 3322

Re: Xadow sleep mode

OK, I found the problem: all is working fine, the problem is the serial monitor: when the processor go into sleep mode, it shuts down also the serial. When it wakes up, the serial port is re-opened and the IDE serial monitor must be close and re-opened. If you put a pause just after the wakeup, and ...
by pizzic
Tue Sep 22, 2015 4:39 am
Forum: Wearables
Topic: Xadow sleep mode
Replies: 2
Views: 3322

Xadow sleep mode

Hi. I'm running the following code on Xadow: void setup() { Serial.begin(9600); while(!Serial.available()); Xadow.init(); delay(2000); Serial.println("Init over"); } void loop() { Serial.println("Sleeping"); delay(1000); Xadow.pwrDown(4000); // sleep for 1000ms Xadow.wakeUp(); // wake up Serial.prin...
by pizzic
Tue Apr 07, 2015 1:12 am
Forum: Wearables
Topic: PIN for external device
Replies: 1
Views: 1227

PIN for external device

Hello.

Quick question: I hava a main board with a serial breakout.
I need to turn on an external device by putting a pin HIGH for two seconds. How can I do it with Xadow?
Do I have the possibility to do this?

Thanks,