Search found 98 matches

by Icing
Tue Dec 21, 2010 2:21 pm
Forum: Arduino & Seeeduino
Topic: Electricity Data Logger
Replies: 5
Views: 3781

Re: Electricity Data Logger

Sorry, what kind of sensor are you using? Could you give us a link?

Steve
by Icing
Mon Oct 18, 2010 4:49 pm
Forum: Bee series & WSN
Topic: usb Arduino, xbe shield, bluetooth bee
Replies: 3
Views: 3657

Re: usb Arduino, xbe shield, bluetooth bee

Hi, I found that with just the inquiry command Serial.print("\r\n+INQ=1\r\n"); in setup, it was enough to keep the device in inquiry mode. Yes, the execution of command STWMOD will be remembered by the Bluetooth Bee, so it is only need one time. However, the INQ should be used every time to make the...
by Icing
Fri Oct 15, 2010 1:15 pm
Forum: Bee series & WSN
Topic: usb Arduino, xbe shield, bluetooth bee
Replies: 3
Views: 3657

Re: usb Arduino, xbe shield, bluetooth bee

Hi, For the hardware connection, please refer to http://www.seeedstudio.com/forum/viewtopic.php?f=18&t=1112&hilit=XBEE For the code, I think after "Serial.begin(38400);" then "Serial.print("\r\n+STWMOD=0\r\n"); Serial.print("\r\n+INQ=1\r\n");" is ok. May this helpful to you, and let me know if you h...
by Icing
Tue Oct 12, 2010 8:49 pm
Forum: Bee series & WSN
Topic: Test Bluetooth Bee on a Mac
Replies: 9
Views: 7080

Re: Test Bluetooth Bee on a Mac

Hi there,

You just need sending command "\r\n+STAUTO=1\r\n" one time,
then Bluetooth Bee will be auto-connected with your PC without setting "\r\n+INQ=1" every time it starts up.

Cheer,

-Icing
by Icing
Tue Oct 05, 2010 11:22 am
Forum: Bee series & WSN
Topic: PIN length
Replies: 1
Views: 2019

Re: PIN length

How long can be the pin in Bluetooth Bee?
It should be exactly 4 characters.
by Icing
Fri Oct 01, 2010 2:28 pm
Forum: Bee series & WSN
Topic: Test Bluetooth Bee on a Mac
Replies: 9
Views: 7080

Re: Test Bluetooth Bee on a Mac

Hi Alessandro,

Have you made it success?

Try to use CR option instead of CR+LF.

Regards,

-Icing
by Icing
Tue Sep 28, 2010 8:56 pm
Forum: Bee series & WSN
Topic: Test Bluetooth Bee on a Mac
Replies: 9
Views: 7080

Re: Test Bluetooth Bee on a Mac

Hi, You can get more on how to use Bluetooth Bee by searching in the forum. Here is the link: http://www.seeedstudio.com/forum/viewtopic.php?f=4&t=687&hilit=bluetoothBee The critical part is to ensure you have sent the right command to the module and it is successfully received. Another question: Th...
by Icing
Fri Sep 17, 2010 2:12 am
Forum: Bee series & WSN
Topic: (Bluetooth bee+Xbee shield+Arduino) How to set Xbee jumpers?
Replies: 1
Views: 2891

Re: (Bluetooth bee+Xbee shield+Arduino) How to set Xbee jumpers?

Hi Yan, Bluetooth Bee and Xbee is compatible in TX,RX,RESET and GND pins. The following info is from http://www.arduino.cc/en/Main/ArduinoXbeeShield With the jumpers in the Xbee position (i.e. on the two pins towards the interior of the board), the DOUT pin of the Xbee module is connected to the RX ...
by Icing
Fri Sep 17, 2010 2:02 am
Forum: Arduino & Seeeduino
Topic: New rainbowduino, where to start?
Replies: 10
Views: 7404

Re: New rainbowduino, where to start?

Hi caskie2010,

Could you tell more about how to use the Rainbowduino, and please check every step as I described.

Good luck,

-Icing
by Icing
Mon Sep 06, 2010 6:47 pm
Forum: Arduino & Seeeduino
Topic: Arduino Mega and Rainbowuino v2.0
Replies: 8
Views: 4669

Re: Arduino Mega and Rainbowuino v2.0

Try to connect TX-RX,and RX to Tx