Search found 138 matches

by rich
Wed Jun 27, 2012 12:19 am
Forum: To Be Classified
Topic: RFBee firmware updating
Replies: 143
Views: 109070

Re: RFBee firmware updating

I have seen other values, but I will find a moment to test again to see if I currently see different values today.
by rich
Tue May 03, 2011 10:24 am
Forum: To Be Classified
Topic: DSO Quad versus Owon HDS1021M
Replies: 2
Views: 2591

Re: DSO Quad versus Owon HDS1021M

The 72mhz number may not be what you think. The current belief is that update firmware will get it to 15mhz usable. This is sampling limited.
by rich
Tue May 03, 2011 10:02 am
Forum: DSO
Topic: how do we order digital probes
Replies: 24
Views: 12810

Re: how do we order digital probes

If you look at some of the other sites selling dso nano's you can find switchable 1x-10x probes with this connector on them.
by rich
Sat Apr 30, 2011 10:09 am
Forum: DSO
Topic: How to make the drive visible under linux in upgrade mode
Replies: 18
Views: 12476

Re: How to make the drive visible under linux in upgrade mode

Mac OS is always trying to write hidden files to usb disks. .Spotlight-V100 .Trashes ._.Trashes .disk .fseventsd maybe disabling this feature using "BlueHarvest" or similar program would resolve issues on mac... but I haven't tried it. DO NOT TRY THIS. I did and it does not work and causes the Mac ...
by rich
Sat Apr 30, 2011 9:45 am
Forum: DSO
Topic: How to make the drive visible under linux in upgrade mode
Replies: 18
Views: 12476

Re: How to make the drive visible under linux in upgrade mode

This is unfortunate. I would have figured being an open source project we would have linux support. I don't run windows on my machine. I'll try to see if I can find a copy of Windows and run it in a VM, but this is a massive inconvenience. I also support modding the firmware (if possible) to have t...
by rich
Fri Apr 29, 2011 9:14 am
Forum: DSO
Topic: How to make the drive visible under linux in upgrade mode
Replies: 18
Views: 12476

Re: How to make the drive visible under linux in upgrade mode

If you need test run I can test on both platforms, I can find a few other platforms as well.

Having an open tool chain is as important to me as having an open device.
by rich
Tue Apr 26, 2011 12:36 pm
Forum: DSO
Topic: DSO Quad App Ideas - Software Defined Radio
Replies: 3
Views: 2946

Re: DSO Quad App Ideas - Software Defined Radio

We were discussing this possibility at lunch today. My quad had just arrived. I also believe we can do a spectrum analyzer as well.
by rich
Tue Apr 26, 2011 12:27 pm
Forum: DSO
Topic: How to make the drive visible under linux in upgrade mode
Replies: 18
Views: 12476

Re: How to make the drive visible under linux in upgrade mode

On mac os it is seen as a disk, but about as long as it takes to open a window to the device is as long as it stays there. At that point it throws an improperly removed drive while it is active error message up. It appears that every time it checks to see if files have changed it disconnects from th...
by rich
Tue Apr 26, 2011 12:17 pm
Forum: DSO
Topic: DSOQuadV2.6 RESOURCE(Update 2012/04/12)
Replies: 290
Views: 379392

Re: DSOQuadV2.6 RESOURCE(Update 2011/4/19)

The DSOQuad HWv2.6 need to upgrade the app/sys/FPGA as the way in the manual because of the BIOS that embeded in the STM32 when Quad was produced . So, DFU-util or dfuse can not be used unless you embeded the related BIOS to the STM32. as on the Mac, it will be grateful for you sharing your experie...
by rich
Tue Apr 26, 2011 12:09 pm
Forum: DSO
Topic: DSO Quad engineering sample bug and firmware upgration
Replies: 70
Views: 63383

Re: DSO Quad engineering sample bug and firmware upgration

Yeah I got mine finally it is working and looks like a great start. The usb disk for updating is a lose for me because it does not work with Linux or Mac os which are all I have easy to use. From what I can see it should not be hard to fix it, but this needs to be fixed. Is there an open source sour...