Search found 2 matches

by mrburen121
Fri May 20, 2016 6:15 pm
Forum: Arduino & Seeeduino
Topic: IR library
Replies: 2
Views: 3746

Re: IR library

Thank you for your reply. I added #include <IRSendRevInt.h> so I can use the code TIMER_ENABLE_INTR; and TIMER_DISABLE_INTR; I tried to enable and disable the interrupt but it don't work. Where do I need to place the enable and disable? #include <IRSendRev.h> #include <IRSendRevInt.h> #define BIT_LE...
by mrburen121
Sun May 15, 2016 5:07 pm
Forum: Arduino & Seeeduino
Topic: IR library
Replies: 2
Views: 3746

IR library

Hello, I found at Github your IRSendRev library . In the examples sending and receiving IR signals are separated. I tried to combine the codes so both my Arduino's can send and receive data (half-duplex). But I whatever I tried it doesn't work. With the code below the Arduino's only sending data and...