Search found 15 matches

by sheepjms
Thu May 19, 2016 10:53 am
Forum: Wio Series
Topic: New Pluggins for Piezo Vibration Sensor
Replies: 1
Views: 2101

Re: New Pluggins for Piezo Vibration Sensor

It is coming soon, boadude!

But before it comes, I think you can make a vibrate sensor with grove interface for your self!No matter analog , digital or PWM signal, just confirm which number of pin of the grove is NC before you connecting.
by sheepjms
Thu May 19, 2016 10:28 am
Forum: Wio Series
Topic: WIO digital outputs not changing
Replies: 3
Views: 2972

Re: WIO digital outputs not changing

Hi rogersan, what is the response under your Test Request? And what is the instruction you post in the test request? 1 and 0 ? or ON and OFF? In fact , even though there are four pins in the digital 0(3V3, GND,and two IO pins) ,some of them may be NC when it is setted as a general digital output, ac...
by sheepjms
Wed May 18, 2016 10:08 am
Forum: Wio Series
Topic: ULB Recipes
Replies: 2
Views: 2502

Re: ULB Recipes

Hi bjarne, the ULB you talked about is what we call Iot system.Cool! here is the attachment of the example project which can implement the ULB you said.Of course you need to code before it runs.Later you may see other ULB projects in the recipes, and you can try to make your own ULB for the recipes ...
by sheepjms
Tue May 17, 2016 11:36 am
Forum: Wio Series
Topic: Sensor data on website
Replies: 4
Views: 3483

Re: Sensor data on website

Hi sheepjms, Thanks a lot. I didn't know these services exist. I played around with freeboard and it worked very well with the Wio Link sensors. But my question wasn't very precise. What I want to do is integrating the sensor data in my own website. That's why I was looking some kind of PHP code. T...
by sheepjms
Tue May 17, 2016 11:26 am
Forum: Wio Series
Topic: wio-cli failed
Replies: 4
Views: 3438

Re: wio-cli failed

Maybe this will help for the same problem: https://github.com/diraimondo/gmusicproxy/issues/35
by sheepjms
Tue May 17, 2016 11:14 am
Forum: Wio Series
Topic: Air Conditioner IR Controller
Replies: 10
Views: 8923

Re: Air Conditioner IR Controller

Hi joshuaguedalia! I'm one member of the Wio team.The advice wassabi gave you is quite useful! Thanks wassabi :D ! Since you are a new learner, I suggest you start with IFTTT , work with some basic function. If you want to try further experiment, you can try the advanced user guide of wio link. Mean...
by sheepjms
Mon May 16, 2016 9:49 am
Forum: Wio Series
Topic: Sensor data on website
Replies: 4
Views: 3483

Re: Sensor data on website

That's a useful and fundamental function for iot project!In fact, you don't need to use PHP to write the website, because there are some website can implement your requirement already.You can try http://dweet.io or http://freeboard.io to send your sensor data on website with graphical vision.It's qu...
by sheepjms
Sat May 14, 2016 12:38 pm
Forum: Wio Series
Topic: [resolved]Cant read output on debug console
Replies: 3
Views: 3423

Re: Cant read output on debug console

You need to OTA the Wio Link at least once to update the firmware to the new one having debugging enabled.Which require you to deploye a private server.If not, please re-flash the Wio Link with the firmware having debugging enabled.one thing should be noticed that the debugging printing will be disa...
by sheepjms
Thu May 12, 2016 3:13 pm
Forum: Wio Series
Topic: #idea Weather station with LED temp without coding
Replies: 2
Views: 3954

Re: #idea Weather station with LED temp without coding

How to store the data on initial state? :)
by sheepjms
Wed May 11, 2016 10:56 am
Forum: Wio Series
Topic: Which Jst battery plug is the correct one?
Replies: 4
Views: 2538

Re: Which Jst battery plug is the correct one?

http://www.seeedstudio.com/depot/JST-2- ... p-649.html
this one is what you need