Search found 19 matches

by Wio
Tue May 24, 2016 4:32 am
Forum: Wio Series
Topic: Can not find Barometer Sensor(BMP180) in iOS app
Replies: 8
Views: 7171

Re: Can not find Barometer Sensor(BMP180) in iOS app

I just got my bmp280 sensor and it Seems that it doesent work with the bmp280 selected.
If I select bmp085 it shows a wrong Temperatur and altitude, not sure with pressure.

Are there any updates or fixes coming???
by Wio
Thu May 12, 2016 7:43 am
Forum: Wio Series
Topic: Is it possible to use arithmetic functions before forwarding
Replies: 6
Views: 5128

Re: Is it possible to use arithmetic functions before forwar

Does this really don't work?
I like how easy the IFTTT thing is but I hate that you touch the borders of so quickly...
by Wio
Sat May 07, 2016 7:00 pm
Forum: Wio Series
Topic: Which Jst battery plug is the correct one?
Replies: 4
Views: 2589

Which Jst battery plug is the correct one?

Is this the correct battery plug:
http://www.seeedstudio.com/depot/JST-2- ... p-649.html

I just got a whole bag of these:
http://www.ebay.de/itm/380809062681?_tr ... EBIDX%3AIT

And they don't fit :(
by Wio
Sat May 07, 2016 6:52 pm
Forum: Wio Series
Topic: Can not find Barometer Sensor(BMP180) in iOS app
Replies: 8
Views: 7171

Re: Can not find Barometer Sensor(BMP180) in iOS app

Still have not understand the exact problem, is the sensor not working? or can't it be selected in the app?
by Wio
Sat May 07, 2016 6:51 pm
Forum: Wio Series
Topic: Programming the Wio
Replies: 5
Views: 3063

Re: Programming the Wio

you can do this very easy with IFTTT nothing else needed than a few apps. There are YouTube videos out there which explain the wio link setup. IFTTT is a simple app which allows to select a lot of sensors and actors and some rules when to make what. It checks the status every 5-20minutes. You just n...
by Wio
Mon May 02, 2016 2:40 am
Forum: Wio Series
Topic: How to make a momentary pulse
Replies: 4
Views: 1822

Re: How to make a momentary pulse

Which times do you plan?
by Wio
Mon May 02, 2016 1:32 am
Forum: Wio Series
Topic: Negative event option
Replies: 3
Views: 1474

Re: Negative event option

What are u using? In IFTTT you can select equal 0 nor a generic digital input. This should work.
by Wio
Mon May 02, 2016 1:21 am
Forum: Wio Series
Topic: Longer Groove Cable needed
Replies: 7
Views: 5161

Re: Longer Groove Cable needed

You can simply cut the wire and solder a wire in between of the wished size. Just make sure you use some heatsshrink for insulation and weatherproofing.
by Wio
Mon May 02, 2016 1:18 am
Forum: Wio Series
Topic: Sleep API
Replies: 1
Views: 1126

Re: Sleep API

Interesting, have you tried other numbers? Does it wake up exactly 90seconds every time? The wio should wake up when it gets another command , so is there maybe something different contacting the device. The biggest number I have used was 20 minutes triggered with IFTTT and the maker channel. This w...
by Wio
Mon May 02, 2016 1:11 am
Forum: Wio Series
Topic: Can not find Barometer Sensor(BMP180) in iOS app
Replies: 8
Views: 7171

Re: Can not find Barometer Sensor(BMP180) in iOS app

I have a spot for the barometer in the i2c section. One for bmp085 and one for bmp280(compatible to bmp180).

I have not tried it because my bmp280 is still on its way to me.