Search found 5 matches

by qxn.c
Thu May 05, 2016 11:47 am
Forum: BeagleBone
Topic: Problem with Motor Bridge Cape
Replies: 19
Views: 24477

Re: Problem with Motor Bridge Cape

FIXED, I think. The problem was on my end with the typos, but anyways, here is what I did to fix it. I enabled BB-UART2 in my uEnv.txt file using commands given by qxn.c. nano /boot/uEnv.txt Add in the following: #for v4.1.x cape_enable=bone_capemgr.enable_partno=BB-UART2 #for v3.8.x cape_enable=ca...
by qxn.c
Fri Apr 22, 2016 1:23 pm
Forum: Wio Series
Topic: WioLink power charging specs
Replies: 1
Views: 1009

Re: WilLink power charging specs

I am interested in outdoor applications for Wio. I plan to used both solar and Li ion batteries. Does the Wio have voltage protection on its charging circuit? Is it possible to connect the JST 2 connector directly to a solar panel bearing in mind that solar panels even at a nominal 5V can result in...
by qxn.c
Fri Apr 22, 2016 12:04 pm
Forum: Wio Series
Topic: Posting more than 1 digit to grove digital display
Replies: 2
Views: 6896

Re: Posting more than 1 digit to grove digital display

There doesn't seem to be a Wio Link forum yet so posting in this one. I'm experimenting with the Wio Link and Grove Digital display (the one with 4 digits) There is an example on how to post a digit (using position and character) using restful API as per the screenshot attached. What I wanted to kn...
by qxn.c
Fri Apr 22, 2016 10:36 am
Forum: BeagleBone
Topic: Problem with Motor Bridge Cape
Replies: 19
Views: 24477

Re: Problem with Motor Bridge Cape

Getting the same error as OP, with very similar setup so far except using BBB and using Debian GNU/Linux 8 2016-01-24 When I try to flash the firmware using (make flash_firmware) I get an error though. I'm relatively new with BBB, so I'm not sure if there are other ways to 'flash the firmware.' Tha...
by qxn.c
Wed Apr 20, 2016 6:37 pm
Forum: Wio Series
Topic: iOS App Crashing on Launch
Replies: 1
Views: 1019

Re: iOS App Crashing on Launch

Hi Nate,

Thank you for your feedback.

Can you try to delete the app and re-install it.

Keep me updated.