Search found 7 matches

by drstoneburg
Fri Jun 28, 2019 6:54 am
Forum: New Product Ideas
Topic: ESP32 motor/stepper/servo board
Replies: 0
Views: 2180

ESP32 motor/stepper/servo board

It would be nice to have a closed loop board I could put on the back of a stepper that would communicate to the controller with BT. And the other GPIO should still be available for add-ons in the vicinity. If it had a built-in 9/10 DOF chip then it would even know where it was in relation to the oth...
by drstoneburg
Fri Jun 28, 2019 6:42 am
Forum: Highlight Projects
Topic: Maixduino for Max (Headroom) robot
Replies: 0
Views: 3051

Maixduino for Max (Headroom) robot

I just received my Maixduino w/Binoc. camera board and 6+1 Mic board for use in an android head (InMoov). I will also need 10DOF board and servo/motor driver boards. I especially like that the Maixduino has ESP32 on board so I can utilize BT for communicating with other parts of the robot, including...
by drstoneburg
Thu May 30, 2019 6:07 am
Forum: Complaints and Suggestions
Topic: 6 + 1 Mic Array (SKU 107990113)
Replies: 1
Views: 4693

6 + 1 Mic Array (SKU 107990113)

Received error, "404 Not Found" when looking for "Sipeed-R6+1_MicArray_Assembly drawing 2018.11.16" or
"Sipeed-R6+1_MicArray_Assembly drawing 2018.11.16". Where are these documents?
by drstoneburg
Thu May 30, 2019 5:39 am
Forum: Complaints and Suggestions
Topic: MAix Binocular Camera Documentation
Replies: 2
Views: 3187

MAix Binocular Camera Documentation

I was looking for the docs on the Binocular Camera and when selecting MAIX Binocular Camera_Assembly drawing 2018.11.29 or MAIX Binocular Camera Schematic 2018.11.29 it comes up with a 404 error. Please send me all the documentation you have on the Binocular camera so I can incorporate it into my pr...
by drstoneburg
Fri Apr 15, 2016 2:38 am
Forum: Wio Series
Topic: #idea Greenhouse aquaponics monitor/controller
Replies: 5
Views: 3984

Re: #idea Greenhouse aquaponics monitor/controller

I have several temp probes and ultra-sonic PCBs, just ordered a I2C expansion card and a servo motor driver (louvers). Also have several 8x relay boards, but ordered some 2x boards for pump control. Sump pump w/float works well in the sump but doesn't do anything for make-up water. My 'real job' is ...
by drstoneburg
Fri Apr 08, 2016 12:23 am
Forum: Wio Series
Topic: #idea Greenhouse aquaponics monitor/controller
Replies: 5
Views: 3984

#idea Greenhouse aquaponics monitor/controller

I plan to use several nodes: 1) Fish tank monitor/controller - temperature/heater, water level/valves, ... 2) Plant bed monitor/controller - temperature, moisture, pH, .... 3) Ambient air monitor - temp, Rh, louver controls, .... 4) Smart Evaporative Cooler - temperature, water pump, fan speed contr...
by drstoneburg
Thu Apr 07, 2016 11:40 pm
Forum: Wio Series
Topic: Got my wio. Rocks!
Replies: 3
Views: 2093

Re: Got my wio. Rocks!

I've had mine a couple of days. I originally ordered them (2) for a friend's greenhouse crop but he got froze out and I haven't heard if he is going to start again. Still, it would be a nice project to get started on myself. Just getting seedlings, good timing.