Search found 7 matches

by ASHTONMARKSON
Tue Mar 29, 2016 10:15 pm
Forum: RePhone
Topic: Using Bluetooth in the arduino IDE?
Replies: 3
Views: 2920

Re: Using Bluetooth in the arduino IDE?

I'll post my continued findings here.... after some debugging I find that despite: bool success = LBTServer.begin((uint8_t*)SPP_SVR); returning true, if(LBTServer.available()) is always false. Further, when I comment the majority of the loop method out, the loop does in fact run and I do so the devi...
by ASHTONMARKSON
Tue Mar 29, 2016 1:15 am
Forum: RePhone
Topic: Does NFC V1 work with Rephone GSMBLE?
Replies: 2
Views: 1855

Re: Does NFC V1 work with Rephone GSMBLE?

good point, so all the xadow modules are "just" i2c then? I should be able to wire a seperate 3.3v to the pin and the 2 i2c wires back to the gsm/bt chip and it would work as "normal"?

Thanks
by ASHTONMARKSON
Tue Mar 29, 2016 1:12 am
Forum: RePhone
Topic: Using bluetooth with Eclipse IDE
Replies: 1
Views: 1029

Re: Using bluetooth with Eclipse IDE

Have you been able to get it working with arduino? I have not been able to get it working at all.
by ASHTONMARKSON
Mon Mar 28, 2016 12:08 am
Forum: RePhone
Topic: Using Bluetooth in the arduino IDE?
Replies: 3
Views: 2920

Re: Using Bluetooth in the arduino IDE?

I can't get the examples to work. Has someone successfully done a walk through? I tried both the client and server .ino files. They compile ok, but there is nothing coming on the serial console and no Bluetooth devices are discoverable by my BT sniffer.
by ASHTONMARKSON
Sun Mar 27, 2016 11:52 pm
Forum: RePhone
Topic: Does NFC V1 work with Rephone GSMBLE?
Replies: 2
Views: 1855

Does NFC V1 work with Rephone GSMBLE?

I ordered an NFC Board (just realized that its the V1), is it possible to connect it to the rephone's main board? The connections are different.
by ASHTONMARKSON
Sun Mar 27, 2016 11:51 pm
Forum: RePhone
Topic: Hash file is not present
Replies: 1
Views: 1041

Re: Hash file is not present

After a few reboots, all worked fine. I'm not sure what the problem was but it works now.
by ASHTONMARKSON
Sun Mar 27, 2016 4:34 am
Forum: RePhone
Topic: Hash file is not present
Replies: 1
Views: 1041

Hash file is not present

Hi,
When installing the drivers on a w10 machine after turning off the device signature step, I get an error when trying to register the MTK USB DEBUG Port driver. It says that it has a bad or not present hash file and it may have been tampered with. Is there a special one for w10 or something?