Search found 37 matches

by seeed86
Sun Feb 28, 2016 4:06 pm
Forum: RePhone
Topic: Event for charger connected
Replies: 3
Views: 1083

Re: Event for charger connected

as you can be noticed, there is such thing on RePhone (it activate mass storage mode on USB connect, and, afair, powers on in that mode even on charger. Although, that code is in bootloader (just like on mobile phones/smartphones). So, AFAIU, you have nothing to do about that in your VXP program (wh...
by seeed86
Sat Feb 27, 2016 2:36 pm
Forum: RePhone
Topic: Re:Phone sends SMS but doesn't receive
Replies: 10
Views: 6829

Re: Re:Phone sends SMS but doesn't receive

Then, it is, probably, just full SIM-card. "Usual" phones can store received SMS both in the internal memory and on SIM-card. Probably RePhone firmware store them in the internal memory and do not delete after writing them's content in the file on internal flash. Unfortunately, I'm a bit busy ATM to...
by seeed86
Sat Feb 27, 2016 3:04 am
Forum: RePhone
Topic: Re:Phone sends SMS but doesn't receive
Replies: 10
Views: 6829

Re: Re:Phone sends SMS but doesn't receive

Isn't it a case, that bot of you has received 20SMS or so (or, even less, in case of some sim-cards)? :)
by seeed86
Thu Feb 25, 2016 4:15 pm
Forum: RePhone
Topic: (TECH) Incoming Ring Tone?
Replies: 11
Views: 4028

Re: (TECH) Incoming Ring Tone?

Actually, RePhone is a (kinda) opensource platform and you're free to edit CreateKit's source code as you wish. Here is code, which is used to work with SMS. Here is for playing audio. And here is for voice calls. And, as far as I see in the code, you're able to hook that events (incoming SMS and ca...
by seeed86
Thu Feb 25, 2016 4:23 am
Forum: RePhone
Topic: (TECH) Upgrading/Flashing RePhone GPS/NFC modules firmware
Replies: 14
Views: 10158

Re: (TECH) Upgrading/Flashing RePhone GPS/NFC modules firmwa

Uhm. Sorry, I just quick-looked at the code, and didn't open commit history :/
by seeed86
Wed Feb 24, 2016 10:29 pm
Forum: RePhone
Topic: (TECH) Upgrading/Flashing RePhone GPS/NFC modules firmware
Replies: 14
Views: 10158

Re: (TECH) Upgrading/Flashing RePhone GPS/NFC modules firmwa

Thanks a lot!
Although, I'm pretty sure, community would like to see the sources of your changes to GPS firmware and, maybe it somehow speedup new "official" release ;)
by seeed86
Wed Feb 24, 2016 1:42 pm
Forum: RePhone
Topic: (TECH) Upgrading/Flashing firmware without Windows
Replies: 5
Views: 1474

Re: (TECH) Upgrading/Flashing firmware without Windows

And yes, thanks for the uploader script for VXPs. Nice thing ;)
by seeed86
Wed Feb 24, 2016 1:27 pm
Forum: RePhone
Topic: (TECH) Upgrading/Flashing firmware without Windows
Replies: 5
Views: 1474

Re: (TECH) Upgrading/Flashing firmware without Windows

And, yes, I need to upgrade the firmware (RTOS), because SeeedStudio member said that it is required to fix issue with debug port (which doesn't work on stock firmware and sends some scrambled output)
by seeed86
Wed Feb 24, 2016 1:18 pm
Forum: RePhone
Topic: (TECH) Upgrading/Flashing firmware without Windows
Replies: 5
Views: 1474

Re: (TECH) Upgrading/Flashing firmware without Windows

Hi! Actually, I exactly talked about "main firmware", which is closed RTOS, and, @dbelam already noticed me about existence of suitable API function , but it is a bin unclear, what actually should be used to flash: API documentation says Calling this function causes the system to reboot immediately ...