Search found 20 matches

by getmemot
Sun Apr 17, 2016 6:24 am
Forum: RePhone
Topic: Can't get Wire to work Xadow GSM
Replies: 2
Views: 1630

Re: Can't get Wire to work Xadow GSM

Oh okay that make senses.

Thanks
by getmemot
Sat Apr 16, 2016 11:24 pm
Forum: RePhone
Topic: Can't get Wire to work Xadow GSM
Replies: 2
Views: 1630

Can't get Wire to work Xadow GSM

For some reason i can't get this example code to work as soon as I switch the codes around on each device it works. Does anyone know what i'm doing wrong? Xadow GSM #include <Wire.h> void setup() { Wire.begin(8); // join i2c bus with address #8 Wire.onReceive(receiveEvent); // register event Serial....
by getmemot
Mon Apr 04, 2016 6:27 am
Forum: RePhone
Topic: GPS for extrem hiker
Replies: 4
Views: 3383

Re: GPS for extrem hiker

How about when the deivce powers on it send the gps location then you switch it off so that will be your interaction, or you can use the pins on the pad as a switch.
by getmemot
Sat Mar 19, 2016 9:28 pm
Forum: RePhone
Topic: Is there way charging the battery GSM
Replies: 1
Views: 1325

Is there way charging the battery GSM

is there any other way of charging the battery with out using the usb i have looked on the .sch and it looks like it can only be done through the USB5V there is a pad that connects to that it located right next to the usb slot i tried to solder a wire to it but the pad is so small i think i shortage...
by getmemot
Tue Mar 08, 2016 8:11 am
Forum: RePhone
Topic: GPS V2 dash missing from Longitude
Replies: 2
Views: 1300

Re: GPS V2 dash missing from Longitude

Oh okay thank you for the reply
by getmemot
Tue Mar 08, 2016 6:51 am
Forum: RePhone
Topic: GPS V2 dash missing from Longitude
Replies: 2
Views: 1300

GPS V2 dash missing from Longitude

So i've updated my firmware and I notice my location was still not correct. Then i've dragged the pin on google maps to my location so I can see the Latitude and Longitude the numbers was correct but there was a missing dash (-x.xxxxx) in the Longitude so it took me to another location. Is there a f...
by getmemot
Sun Mar 06, 2016 3:30 am
Forum: RePhone
Topic: (TECH) General Flashing Guide
Replies: 2
Views: 2516

Re: (TECH) General Flashing Guide

So what is this for?
https://github.com/sthaugen/Rephone-KL02-swd

does this not show you how to update the GPS v2 firmware?
by getmemot
Sat Mar 05, 2016 3:28 am
Forum: RePhone
Topic: Xadow GSM+BLE Power On/OFF
Replies: 11
Views: 3674

Re: Xadow GSM+BLE Power On/OFF

I brought the following from ebay

Universal 3.7V 20C 1000mAh
by getmemot
Sat Mar 05, 2016 3:00 am
Forum: RePhone
Topic: Xadow GSM+BLE Power On/OFF
Replies: 11
Views: 3674

Re: Xadow GSM+BLE Power On/OFF

Current i have my battery connected to the VCC and GND pin and it works fine for me and it also charges the battery.
by getmemot
Sat Mar 05, 2016 2:49 am
Forum: RePhone
Topic: GPSv2 inaccuracy
Replies: 30
Views: 24893

Re: GPSv2 inaccuracy

I can seem to to get the program on the ESP8266 i have the following error below I have a arduino uno i have connected the follow I have removed the chip from the UNO and connected it up the following Arduino UNO ESP8266(ESP-12F) RX -----------> RX (Logic Level Shifter Converter) TX -----------> TX ...