Search found 19 matches

by alexandru.m.ghe
Sun Mar 27, 2016 6:51 pm
Forum: RePhone
Topic: Access the GPIO Pins based on Different IDEs
Replies: 3
Views: 8577

Re: Access the GPIO Pins based on Different IDEs

Without 'D'

Code: Select all

const int buttonPin = 3;    // button pin on RePhone GSM_Breakout pad A1
by alexandru.m.ghe
Sat Feb 27, 2016 2:00 pm
Forum: RePhone
Topic: Re:Phone sends SMS but doesn't receive
Replies: 10
Views: 6679

Re: Re:Phone sends SMS but doesn't receive

I think yes.
by alexandru.m.ghe
Sat Feb 27, 2016 12:13 am
Forum: RePhone
Topic: Re:Phone sends SMS but doesn't receive
Replies: 10
Views: 6679

Re: Re:Phone sends SMS but doesn't receive

I have the exact same problem.
It was working for some time and then it stopped working.
I used the SMS example, checked SIM and it's ok, but nothing.
by alexandru.m.ghe
Sun Feb 14, 2016 4:32 pm
Forum: RePhone
Topic: Serial Comunication via USB not working
Replies: 5
Views: 2891

Re: Serial Comunication via USB not working

You can update the firmware, for me updating the firmware solved this problem
by alexandru.m.ghe
Sun Feb 14, 2016 4:21 pm
Forum: RePhone
Topic: [Question]How to use GRPS on RePhone
Replies: 4
Views: 1687

Re: [Question]How to use GRPS on RePhone

Actually in the example it's HTTP GET not POST.
by alexandru.m.ghe
Sun Feb 14, 2016 4:13 pm
Forum: RePhone
Topic: (TECH) Xadow GSM+BLE module restarts with SIM
Replies: 4
Views: 1667

Re: (TECH) Xadow GSM+BLE module restarts with SIM

Hello,

I had the same problem. The battery must have 3.3 ~ 4.2V(no SIM)/3.5 ~ 4.2V(with SIM).
You can replace the battery
by alexandru.m.ghe
Fri Feb 12, 2016 2:07 pm
Forum: RePhone
Topic: GSM Signal strength
Replies: 5
Views: 2210

Re: GSM Signal strength

Ok and how can i use it in Arduino ?
by alexandru.m.ghe
Wed Feb 10, 2016 2:53 pm
Forum: RePhone
Topic: GSM Signal strength
Replies: 5
Views: 2210

GSM Signal strength

Hello,

How can i get gsm signal strength ?
by alexandru.m.ghe
Sun Feb 07, 2016 2:18 pm
Forum: RePhone
Topic: (TECH) Gate Command
Replies: 4
Views: 1891

Re: (TECH) Gate Command

An optocoupler (4N35) before the relay could help you.

Like this:
Relay control.JPG
by alexandru.m.ghe
Sat Feb 06, 2016 6:12 pm
Forum: RePhone
Topic: SSD1331 Oled display and RePhone
Replies: 14
Views: 5268

Re: SSD1331 Oled display and RePhone

Even more, i updated the example in the Adafruit_SSD1331 library in order to work by default with Rephone. You only need to change the pins, if you want.

Please notice, those libraries are for Arduino IDE for Rephone.