Search found 157 matches

by dbelam
Wed Mar 27, 2019 4:23 am
Forum: Hardware Products for AIoT Applications
Topic: Maix Dock help
Replies: 1
Views: 1658

Maix Dock help

Hi guys!

Feel free to add your questions too!

Let me start: I started the board with micropython, but the displayed image has pretty ugly colors.
I changed the image mode from RGB565 to YUV, it became even greener.

Anyone having better results?
by dbelam
Thu May 19, 2016 2:33 am
Forum: RePhone
Topic: SDK Required
Replies: 6
Views: 3894

Re: SDK Required

You can add the solution, it won't help - the GPS module, not the rephone has bad firmware. You can do anything with the rephone, it will always show the bad value because the GPS sends the bad value. Reflash the GPS module itself, not rephone.
by dbelam
Tue May 17, 2016 4:52 am
Forum: RePhone
Topic: Reflash Xadow Duino
Replies: 4
Views: 3809

Re: Reflash Xadow Duino

If you are using avrisp, just choose the atmega32 profile (if it's the microcontroller) and reflash it As an atmega.
by dbelam
Sun May 15, 2016 3:00 pm
Forum: RePhone
Topic: Reflash Xadow Duino
Replies: 4
Views: 3809

Re: Reflash Xadow Duino

It's just plain Arduino. Try reflash bootloader, hopefully it goes with the usb, if not, another Arduino can act As a programmer, and you can reflash via isp port.
by dbelam
Sat May 14, 2016 2:55 am
Forum: RePhone
Topic: Applications for rePhone
Replies: 1
Views: 2260

Re: Applications for rePhone

Neat stuff mate! Budapest in Hungary has a similar bus tracking system, called Futár. You can check the buses realtime. Pretty cool thing. Check it out here: http://futar.bkk.hu/ One question about the bridge: is that somewhat a safety-critical application, or just commercial sensors are allowed to ...
by dbelam
Sat May 14, 2016 2:48 am
Forum: RePhone
Topic: Newbie...Doubts
Replies: 1
Views: 1783

Re: Newbie...Doubts

If you are completely newbie, then no one can provide a step-by-step tutorial.
It's just way too much. Hacking rephone HW is not your level. If you can't solder a small amplifier to the 2 output channel on the breakout board, don't start with an advanced device like this.
by dbelam
Wed May 11, 2016 3:00 am
Forum: RePhone
Topic: Raspberry Pi And Rephone
Replies: 4
Views: 3916

Re: Raspberry Pi And Rephone

You probably can't build on raspberry, sorry.
And to connect the 2? Probably uart, because the rephone only works As i2c master.
by dbelam
Sun May 08, 2016 6:46 pm
Forum: RePhone
Topic: SDK Required
Replies: 6
Views: 3894

Re: SDK Required

Oh you also found the GPS bug.
You have to get the new firmware and reflash the GPS module, a whole thread is about it, you can find every answer there:
http://www.seeedstudio.com/forum/viewto ... =71&t=6684
by dbelam
Sat May 07, 2016 3:11 pm
Forum: RePhone
Topic: Hello, Where to start?
Replies: 3
Views: 2480

Re: Hello, Where to start?

If you are new to embedded, I'd suggest start with the Arduino, there are a bunch of sample codes and projects, also libraries for arduino-compatible libraries.

And the reos has already working power and screen management, the gui framework is the next :)
by dbelam
Sat May 07, 2016 3:06 pm
Forum: RePhone
Topic: SDK Required
Replies: 6
Views: 3894

Re: SDK Required

Which sdk? The one for the Eclipse with the Mediatek SDK?