Search found 33 matches

by jinyuan.weng
Mon Mar 28, 2016 9:40 am
Forum: RePhone
Topic: (TECH) Arduino IDE - Using Interrupts
Replies: 6
Views: 4268

Re: (TECH) Arduino IDE - Using Interrupts

Hi,
You can make reference to ...\Arduino_IDE_for_RePhone\workspace\eint_test.
by jinyuan.weng
Fri Mar 25, 2016 3:34 pm
Forum: RePhone
Topic: (TECH) Drawing an image to screen
Replies: 1
Views: 1134

Re: (TECH) Drawing an image to screen

Hi, I know a way to display image in eclipse. You can make reference to ...\eclipse\LINKIT_ASSIST_SDK\examples\API\Graphic_SpinningLine. It is using resource editor tool to convert image, and load the image buffer data to storage. Then get the buffer data by id and display it on screen. You can chec...
by jinyuan.weng
Thu Mar 17, 2016 4:08 pm
Forum: RePhone
Topic: Using Bluetooth in the arduino IDE?
Replies: 3
Views: 2873

Re: Using Bluetooth in the arduino IDE?

Hi,
Maybe you can make reference to ...\Arduino_IDE_for_RePhone\hardware\arduino\mtk\libraries\LBT.
by jinyuan.weng
Mon Mar 14, 2016 6:36 pm
Forum: RePhone
Topic: (TECH) use FastLED Library with Rephone via Xadow Duino
Replies: 2
Views: 2270

Re: (TECH) use FastLED Library with Rephone via Xadow Duino

Hi Kathryn, The Xadow Duino is similarly to Arduino Leonardo that the core is ATmega32u4, i think you can use the FastLed library and example. But there is a MOSFET switch on pin VLED, don't forget to open it when use this pin to supply power. And then you need to care about the communicate protocol...
by jinyuan.weng
Mon Mar 14, 2016 5:02 pm
Forum: RePhone
Topic: (TECH) RePhone with LED Matrix
Replies: 17
Views: 9972

Re: (TECH) RePhone with LED Matrix

Hi,
If you check the button by read pin value, all the digital pin can be used.
But if you check the button by interrupt, pin INT1/E1/GPIO18, INT2/E2/GPIO13, A2/GPIO1, A3/GPIO2 can be used.
by jinyuan.weng
Fri Mar 11, 2016 9:22 am
Forum: RePhone
Topic: (TECH) Arduino IDE - Using Interrupts
Replies: 6
Views: 4268

Re: (TECH) Arduino IDE - Using Interrupts

Hi Gary,
I remember the Github fix a bug about interrupts.
Maybe you can update the IDE and try it again.
:)
by jinyuan.weng
Thu Mar 10, 2016 10:37 am
Forum: RePhone
Topic: GPRS Library
Replies: 4
Views: 4224

Re: GPRS Library

Hi,
I found these is a example about GPRS that is ..\Arduino_IDE_for_RePhone\hardware\arduino\mtk\libraries.
Maybe you can make reference to it.
by jinyuan.weng
Wed Mar 09, 2016 11:50 am
Forum: RePhone
Topic: (TECH) Couldn't install Xadow Duino Driver
Replies: 5
Views: 3050

Re: (TECH) Couldn't install Xadow Duino Driver

Hi,
I found Github about Xadow Duino driver, maybe you can try it again.
by jinyuan.weng
Wed Mar 09, 2016 11:44 am
Forum: RePhone
Topic: (TECH) Anyone want a keyboard for sending SMS messages?
Replies: 9
Views: 5613

Re: (TECH) Anyone want a keyboard for sending SMS messages?

Hi,
I download the code, and it can type SMS, but I found it can't receive the SMS when send out a SMS.
by jinyuan.weng
Tue Mar 08, 2016 5:53 pm
Forum: RePhone
Topic: (TECH) 5x7 LED source code won't build
Replies: 5
Views: 2834

Re: (TECH) 5x7 LED source code won't build

Hi,
I found the API of 5x7 led, and it is run on Arduino. Maybe you can make a reference.