Search found 7 matches

by m.duerr
Sun Feb 21, 2016 2:25 am
Forum: RePhone
Topic: RePhone analog read problem
Replies: 9
Views: 4726

Re: RePhone analog read problem

Running the adc_test sketch and connecting A3 (breakout E/1) with 2V8 (C/5) with GND the value goes down from 1023 to zero.
This worked in my case also when the display was connected (but not in use). The touch pad is a i2c device so you should be able to use it simultainiously with the ADC.
by m.duerr
Wed Feb 17, 2016 4:15 am
Forum: RePhone
Topic: RePhone analog read problem
Replies: 9
Views: 4726

Re: RePhone analog read problem

That's it! Thank you! Four lines of the file "hardware/arduino/mtk/cores/arduino/wiring_analog.c" were updated, like described here. https://github.com/Seeed-Studio/Arduino_IDE_for_RePhone/commit/3ead745d99fa94cc8632c19fb4e8d4b4c2e11ebb I edited these lines of this file inside my IDC folder and it w...
by m.duerr
Tue Feb 16, 2016 1:58 am
Forum: RePhone
Topic: RePhone analog read problem
Replies: 9
Views: 4726

Re: RePhone analog read problem

Hi jianzhang.su, thank your for the advice. I tested the adc_test.ino script. Connecting A3 (breakout E/1) with 2V8 (C/5) or GND has no effect. First i tried the adc_test.ino script with the complete assembled RePhone. For a second test i connected the Xadow GSM+BLE only with the Xadow GSM Breakout....
by m.duerr
Sun Feb 07, 2016 4:04 am
Forum: RePhone
Topic: https_test test program not working
Replies: 4
Views: 1666

Re: https_test test program not working

The scirpt waits for an input. You simply have to press a key on your keyboard.

I made a test with my thingspeak account.

I replaced the URL like this.
#define TEST_URL "http://api.thingspeak.com/update?key=Y O U R K E Y &field1=5"

It works fine and is very simple!
by m.duerr
Sat Feb 06, 2016 5:02 am
Forum: RePhone
Topic: RePhone analog read problem
Replies: 9
Views: 4726

Re: RePhone analog read problem

Hello!

Which pins shown here

http://www.seeedstudio.com/wiki/Xadow_G ... e_Overview

can i use for reading analog values.

Would someone please give me a short example sketch (Arduino IDE) with the analogRead() function?
by m.duerr
Sun Jan 31, 2016 1:34 am
Forum: RePhone
Topic: (TECH) Unable to falsh Adrunio IDE firmware
Replies: 14
Views: 5737

Re: (TECH) Unable to falsh Adrunio IDE firmware

I had the same problem but after several trials an errors now it works - no reason why. Maybe these advices help to avoid or overcome the problem: - install the drivers as admin. - be shure, that the battery has enough power. - run "\Arduino_IDE_for_RePhone-master\drivers\mtk\UninstallDriver.exe" to...
by m.duerr
Sun Jan 24, 2016 6:31 am
Forum: RePhone
Topic: RePhone: how to flash the Firmware for Arduino IDE ?
Replies: 11
Views: 7708

RePhone: how to flash the Firmware for Arduino IDE ?

I assembled my RePhone. Everything (touch screen and so on) is working fine. Then, like described here http://www.seeedstudio.com/wiki/Arduino_IDE_for_RePhone_Kit i installed the drivers. Both com ports are listed in the device manager. Next i tried to update the firmware but failed: - My RePhone wa...