Search found 9 matches

by Spetznatz1
Tue Feb 09, 2016 8:32 pm
Forum: RePhone
Topic: Testing Sensorboards
Replies: 5
Views: 2176

Re: Testing Sensorboards

I had a similar problem and then I made sure to carefully disconnect the sensor board then reconnect it making sure the connector cable is fully seated, (make sure you turn off the phone first and probably disconnect the battery as well before doing this). On the subject of the sensors, I wondered i...
by Spetznatz1
Tue Feb 09, 2016 8:24 pm
Forum: RePhone
Topic: Rephone Audio -> sound very low
Replies: 11
Views: 6266

Re: Rephone Audio -> sound very low

My speaker and microphone seem to work pretty good, but do I need to upload some music or sounds for the ringer? When I call my RePhone and it receives the call it doesn't make a sound.
How exactly do I upload music or sounds?
by Spetznatz1
Fri Feb 05, 2016 12:16 pm
Forum: RePhone
Topic: (TECH) Useable SIM cards?
Replies: 11
Views: 10850

Re: (TECH) Useable SIM cards?

That sounds pretty good. I just want something cheap to operate my RePhone, for experimentation. Did you order a SIM card online or go into a store? Everywhere I've been I haven't seen just SIM cards for sale. It's like they want me to buy a phone. I'd hate to pay out $20 for some crap phone just fo...
by Spetznatz1
Mon Feb 01, 2016 8:40 pm
Forum: RePhone
Topic: (TECH) Useable SIM cards?
Replies: 11
Views: 10850

(TECH) Useable SIM cards?

I wondered if anyone knew what specific SIM cards will work with the RePhone? I'm located in the US, and I currently use Verizon, (which is a CDMA carrier, not GSM), and I just wanted to get a pre-paid SIM card to put in my RePhone. I certainly don't want to go about getting a SIM card or two only t...
by Spetznatz1
Mon Feb 01, 2016 6:51 am
Forum: RePhone
Topic: Precute paper schematic
Replies: 5
Views: 2112

Re: Precute paper schematic

That's a great idea. I'd also like to see a pattern for the larger, (or longer case), version as well. I saw an example of one in the video Seeed made for Kickstarter. I would love this to house my components from the expansion kit. The regular case isn't big enough for the extra modules. Mayber I'l...
by Spetznatz1
Mon Feb 01, 2016 4:07 am
Forum: RePhone
Topic: Rephone doesn't see sim card
Replies: 33
Views: 16357

Re: Rephone doesn't see sim card

In regards to the SIM issue, can anyone tell me what carriers in the US has SIM cards that work in the RePhone?? I'm primarily looking for a SIM card from a prepaid, or no contract service. I am on Verizon and I just want to use this phone for experimentation purposes firstly.
by Spetznatz1
Sun Jan 31, 2016 10:04 pm
Forum: RePhone
Topic: (TECH) Expansion Pack????
Replies: 0
Views: 1117

(TECH) Expansion Pack????

Can someone do a tutorial, (preferably video like YouTube), on setting up the expansion pack pieces?? I got one with my RePhone Create kit, and so far I've been able to play with the little LED matrix board, (although I'm not sure how to implement uses for it). I've also used the Basic Sensors board...
by Spetznatz1
Mon Jan 25, 2016 9:13 pm
Forum: RePhone
Topic: Any update on Kickstarter shipments?
Replies: 8
Views: 3694

Re: Any update on Kickstarter shipments?

I have received a couple of emails from Seeed, and they've given me a couple of different tracking numbers. One of which must be someone else's because it shows that it is near its destination but that destination is halfway across the US from me. The other tracking number still just shows "shipping...
by Spetznatz1
Sat Jan 23, 2016 11:21 am
Forum: RePhone
Topic: Any update on Kickstarter shipments?
Replies: 8
Views: 3694

Re: Any update on Kickstarter shipments?

I got the same reward and my tracking number says the same thing, "shipping information..." And it says "shipping label created", but so far it hasn't moved according to USPS for over two days??? I guess they haven't dropped it off at the post office yet. What I thought was strange was that I had th...