Search found 13 matches

by kaktus.martin
Fri Jan 15, 2016 4:52 am
Forum: RePhone
Topic: (TECH) Touchscreen Xadow connection clarifications
Replies: 3
Views: 1973

Re: Touchscreen Xadow connection clarifications

#A look at the datasheet would give you clarity... why people can't do that on your own?

Look at the attachment and post the answer at your own question...
by kaktus.martin
Sun Jan 10, 2016 10:23 am
Forum: RePhone
Topic: Missing Symbols in Firmware?
Replies: 12
Views: 5511

Re: Missing Symbols in Firmware?

Since I know that not all function can be called out of a sub thread, I wrote my own functions where it doesn't matter where you call the apis.... I uploaded you an example in the attachement. Maybe the same problem exists in the Arduino IDE (I'm using Eclipse)... because I saw that in the file ../E...
by kaktus.martin
Sun Jan 10, 2016 12:37 am
Forum: RePhone
Topic: Missing Symbols in Firmware?
Replies: 12
Views: 5511

Re: Missing Symbols in Firmware?

and most APIs are only available to the main
thread
Ah okay, thanks for your answer... is somewhere a list which API's can only be called from the main thread?
by kaktus.martin
Sat Jan 09, 2016 10:17 am
Forum: RePhone
Topic: Missing Symbols in Firmware?
Replies: 12
Views: 5511

Re: Missing Symbols in Firmware?

bakhdaulet wrote:Use this code
I don't wan't to use a timer function, my question ist why the function can't be called out of a thread?!?
by kaktus.martin
Fri Jan 08, 2016 5:10 am
Forum: RePhone
Topic: Rephone doesn't see sim card
Replies: 33
Views: 15474

Re: Rephone doesn't see sim card

I figured it out... I always called the api from a sub thread, but some api's can only be called from the main thread, my sim card is now detected correctly.
by kaktus.martin
Fri Jan 08, 2016 5:09 am
Forum: RePhone
Topic: Missing Symbols in Firmware?
Replies: 12
Views: 5511

Re: Missing Symbols in Firmware?

Both shutdown and reboot work fine here. I used the unmodified demo code for testing - did you flash the SDK version of the firmware with the Firmware updater? Its different from the one with the arduino ide. I Think I figured something out, here is my example code: #include "vmsystem.h" #include "...
by kaktus.martin
Fri Jan 08, 2016 3:21 am
Forum: RePhone
Topic: Missing Symbols in Firmware?
Replies: 12
Views: 5511

Re: Missing Symbols in Firmware?

So I tried it after getting Home from work - seems like the Arduino firmware misses a lot of symbols - probably those that haven't been directly implemented. Using the eclipse IDE with the SDK however allows me to access those API calls. Tried the functions with with Eclipse und the SDK 2.0.46, the...
by kaktus.martin
Thu Jan 07, 2016 12:02 pm
Forum: RePhone
Topic: Setting Pullup/Pulldown Resistors
Replies: 0
Views: 2310

Setting Pullup/Pulldown Resistors

I'm think I'm a little bit out of luck..... today I tried to program Pull UP/DOWN resitors of the pins but it doesn't worked for me. Here is my example code where I try to pullup the internal resistor of GPIO49. Other pins doesn't worked also .... #include "vmsystem.h" #include "vmthread.h" #include...
by kaktus.martin
Mon Jan 04, 2016 12:46 pm
Forum: RePhone
Topic: Rephone doesn't see sim card
Replies: 33
Views: 15474

Re: Rephone doesn't see sim card

Hi kaktus,

have you tried disable the PIN as blkhawk suggested above?
Yes, I have disabled the pin in the SIM card with my smartphone...
by kaktus.martin
Mon Jan 04, 2016 5:02 am
Forum: RePhone
Topic: Rephone doesn't see sim card
Replies: 33
Views: 15474

Re: Rephone doesn't see sim card

I have the same problem, the SIM card can't be detected. Bending the pins a little bit changed nothing. The sim card works fine in my Samsung Galaxy S3 Smartphone. The function VMINT number_count = 0; number_count = vm_gsm_sim_get_card_count(); returns the value "-103". Which I think it means: #defi...