Search found 12 matches

by contact.ggiordano
Fri Mar 25, 2016 8:23 pm
Forum: Grove
Topic: No data with GSR sensor serial monitor
Replies: 3
Views: 2330

Re: No data with GSR sensor serial monitor

SOLVED. Noobish mistake. I didn't upload the thing. How can I show the plot of the data? The plotter doesn't seem to work
by contact.ggiordano
Fri Mar 25, 2016 6:56 pm
Forum: Grove
Topic: No data with GSR sensor serial monitor
Replies: 3
Views: 2330

Re: No data with GSR sensor serial monitor

already done and no change was detected. I also deleted the buzzer code to save space.
I also installed the driver for the board.
I made a new sketch with an easy serial.print("hi"); and it doesn't work. So the problem could be at the base.
by contact.ggiordano
Fri Mar 25, 2016 6:12 pm
Forum: Grove
Topic: No data with GSR sensor serial monitor
Replies: 3
Views: 2330

No data with GSR sensor serial monitor

Hello,
I have this version of arduino
http://hobbycomponents.com/featured/98- ... -usb-cable
linked with a grovehat via an analog port.
I pasted the code in the sketch and executed but I can't see nothing in the serial monitor. Why?
by contact.ggiordano
Sat Jan 02, 2016 4:57 am
Forum: Grove
Topic: How can I create an excel from grove gsr?
Replies: 2
Views: 2522

Re: How can I create an excel from grove gsr?

I appreciated your answer. It was useful and supportive
by contact.ggiordano
Thu Dec 31, 2015 11:20 pm
Forum: Grove
Topic: Differences between accelerometers
Replies: 2
Views: 1762

Re: Differences between accelerometers

So the one you posted it's even more precise than this?
http://www.seeedstudio.com/wiki/Grove_- ... C2%B11.5g)
It isn't displayed the resolution of this product on the datasheet
by contact.ggiordano
Thu Dec 31, 2015 3:04 am
Forum: Grove
Topic: Possible problems between arduino nano and grove uart wifi
Replies: 1
Views: 1923

Possible problems between arduino nano and grove uart wifi

I'm afraid there will be problem. Does it require some specific programming because the USB communication uses the same serial lines?
by contact.ggiordano
Wed Dec 30, 2015 7:40 pm
Forum: Grove
Topic: How can I create an excel from grove gsr?
Replies: 2
Views: 2522

How can I create an excel from grove gsr?

I'm wondering how did they create charts on the wiki http://www.seeedstudio.com/wiki/Grove_-_GSR_Sensor
Are there other ways to store data?
by contact.ggiordano
Tue Dec 29, 2015 10:13 pm
Forum: Arduino & Seeeduino
Topic: Is arduino nano enough powerful to handle 4 sensors?
Replies: 0
Views: 2236

Is arduino nano enough powerful to handle 4 sensors?

I'm going to attach a gsr, hr, temperature, accelerometer sensor to it though a grovehat. My fear is that some problems might arise.
I'm also going to attach a uart wifi module.
by contact.ggiordano
Mon Dec 28, 2015 8:25 pm
Forum: Grove
Topic: Temperature sensor for skin
Replies: 1
Views: 1253

Temperature sensor for skin

Which sensor is the most suitable for skin contact? And also has a high precision.
by contact.ggiordano
Mon Dec 28, 2015 5:47 am
Forum: Wearables
Topic: Differences between xadow duino and xadow main board
Replies: 0
Views: 3419

Differences between xadow duino and xadow main board

which are the differences? Do you think the duino can handle the data coming from a gsr, hr, accelerometer and temperature sensors?