Search found 8 matches

by ThomasCaspari
Wed Jun 01, 2016 8:09 pm
Forum: DSO
Topic: DSO203 GCC APP - Community Edition (2.51+SmTech1.8+Fixes)
Replies: 698
Views: 555451

DFU issues

DFU always has been kind of funny. I once had a problem (not with wildcat, but with gabonator) reinstalling: always got an .err. Needed to reinstall because by accident I overwrote part of the code. Solution was: install something completely different into the same slot, and then try again. Which in...
by ThomasCaspari
Fri May 20, 2016 5:03 pm
Forum: DSO
Topic: DSO203 GCC APP - Community Edition (2.51+SmTech1.8+Fixes)
Replies: 698
Views: 555451

Re: DSO203 GCC APP - Community Edition (2.51+SmTech1.8+Fixes

Dear Wildcat, I see, the problem was that I misunderstood the concept, and there's no system fault at all. Using manual trigger level truly solved the problem for me. For me it is absolutely desirable to display pulsating DC "as is", as currently I mainly measure PPM and PWM signals in lipo powered ...
by ThomasCaspari
Thu May 19, 2016 4:13 pm
Forum: DSO
Topic: DSO203 GCC APP - Community Edition (2.51+SmTech1.8+Fixes)
Replies: 698
Views: 555451

Re: DSO203 GCC APP - Community Edition (2.51+SmTech1.8+Fixes

Dear Wildcat, thanks for your quick reply. After reading your words, I suspect that I might have a hardware problem. After investigating a bit further, I was able to break it down to the use of "NORML" trigger mode, as I usually leave it to "AUTO" and it gets switched to "NORML" in A&B mode, just as...
by ThomasCaspari
Thu May 19, 2016 1:03 am
Forum: DSO
Topic: DSO203 GCC APP - Community Edition (2.51+SmTech1.8+Fixes)
Replies: 698
Views: 555451

Re: DSO203 GCC APP - Community Edition (2.51+SmTech1.8+Fixes

Dear folks, just wanted to report a minor bug I came across in wc3.4 and wc5.1 (just updated to 5.1 - fantastic work wildcat!!!). My setup: HW 2.70 with DFU 3.11C, sys 1.52, alterbios 0.4 (stock except alterbios) Minor bug I just found: When in "A&B" trigger mode, signal sometimes freezes (Ch.B) or ...
by ThomasCaspari
Mon Sep 21, 2015 3:45 am
Forum: DSO
Topic: DSO203 GCC APP - Community Edition (2.51+SmTech1.8+Fixes)
Replies: 698
Views: 555451

Re: DSO203 GCC APP - Community Edition (2.51+SmTech1.8+Fixes

@roger: although slightly off-topic in this thread: sounds interesting, feel free to provide me those Apollo programming inks you wrote about.
by ThomasCaspari
Mon Sep 21, 2015 12:15 am
Forum: DSO
Topic: DSO203 GCC APP - Community Edition (2.51+SmTech1.8+Fixes)
Replies: 698
Views: 555451

Re: DSO203 GCC APP - Community Edition (2.51+SmTech1.8+Fixes

You are talking about a custom version of the package which would require ongoing effort to maintain in subsequent versions and would only work on the 8GB hardware. Did I really miss the point so much? As far as I understood, compatibility with PAWN is a basic feature of the 4 slot version which is...
by ThomasCaspari
Sun Sep 20, 2015 9:29 pm
Forum: DSO
Topic: DSO203 GCC APP - Community Edition (2.51+SmTech1.8+Fixes)
Replies: 698
Views: 555451

Re: DSO203 GCC APP - Community Edition (2.51+SmTech1.8+Fixes

@Roger: this was just a question. I don't think I need to justify this, but in fact I do not always need the high precision of Wildcat's version and in such cases prefer the more intuitive interface of the factory app. I've also been thinking about altering the factory app because I like the interfa...
by ThomasCaspari
Sun Sep 20, 2015 5:44 pm
Forum: DSO
Topic: DSO203 GCC APP - Community Edition (2.51+SmTech1.8+Fixes)
Replies: 698
Views: 555451

Inquiry about 3-slot version W4.4

...would it be possible to generate a 3-slot version loading into slot 2 that's still compatible with PAWN? For some reason I want to keep original app in slot 1 (I use the fourpack version PLUS A1 1.10 which completely fits into first slot), W4.4 in slot 2 and PAWN in slot 4 (HW 2.70, 2MB version, ...