Search found 23 matches

by 92421
Sat Jan 30, 2016 1:53 am
Forum: RePhone
Topic: (TECH) Unable to falsh Adrunio IDE firmware
Replies: 14
Views: 6033

Re: (TECH) Unable to falsh Adrunio IDE firmware

my os
windows 10 32-bit
on dell laptop

maybe you habe problems with the
mtk usb debug port and
mtk usb modem port ?

the install program do not work on my system
i must install over device manager and
manual call the inf file
over
append legacy hardware
and choose the inf file with the explorer
by 92421
Fri Jan 29, 2016 11:31 pm
Forum: RePhone
Topic: (TECH) Unable to falsh Adrunio IDE firmware
Replies: 14
Views: 6033

Re: Unable to falsh Adrunio IDE firmware

usb disconnect rebootshort - no led firmwareupdater start choose rephone klick download usb connect if you see flash drive - wrong if you see com ports - right thats all usb disconnect usb connect if you see flash drive - drive is empty now you can upload : RePhone Create Kit VXP or a aduino sketch ...
by 92421
Thu Jan 28, 2016 4:56 pm
Forum: RePhone
Topic: (TECH)arduinoprogram demolition
Replies: 3
Views: 1372

Re: (TECH)arduinoprogram demolition

thanks for your answer so i make a lot of tests but every times the same - the audio stops it is the original audio example without a change i changed one time the music.mp3, but the same happends with and also without usb connect my mp3 length is 6 sec if i start the serial monitor i see that the a...
by 92421
Thu Jan 28, 2016 1:16 am
Forum: RePhone
Topic: (tech)install LinkIt Assist SDK on win10
Replies: 2
Views: 1191

(tech)install LinkIt Assist SDK on win10

hi, i want to install eclipse + linkit sdk on a windows 10 system the eclipse indigo installation works correct but when i try to install LinkIt Assist SDK i have different problems eclipse shows this in console info "Failed to locate LinkIt Assist SDK 2.0, please reinstall the SDK." the subdirector...
by 92421
Mon Jan 25, 2016 11:13 pm
Forum: RePhone
Topic: (TECH)arduinoprogram demolition
Replies: 3
Views: 1372

(TECH)arduinoprogram demolition

hi
i upload the rephone audio example
copy the file music.mp3
then i start the program
the program is working
it is a endless loop

but after different repeats - 5 to 10 or more
the program stops

after a reset
the same result

an idea ?

greetings
by 92421
Sun Jan 24, 2016 3:36 am
Forum: RePhone
Topic: rephone future with mre
Replies: 0
Views: 1510

rephone future with mre

rephone future with mre
follow this link and read
http://mre.mediatek.com/en

what means this

greetings
by 92421
Fri Jan 22, 2016 1:43 am
Forum: RePhone
Topic: Rephone doesn't see sim card
Replies: 33
Views: 15400

Re: Rephone doesn't see sim card

for me resolved
disable pin code in a smartphone
i have a german o2 prepaid
by 92421
Fri Jan 22, 2016 1:40 am
Forum: RePhone
Topic: rephone mess no sim
Replies: 1
Views: 834

Re: rephone mess no sim

resolved
disable pin code in a smartphone
i have a german o2 prepaid
by 92421
Fri Jan 22, 2016 12:42 am
Forum: RePhone
Topic: Flash original firmware
Replies: 3
Views: 2007

Re: Flash original firmware

i have now the same problem after firmware update
touchscreen is black

can not find the file
RePhone_Create_Kit_VXP
link does not work - only a png file