Search found 5 matches

by sebastian5
Mon Jul 20, 2015 6:19 pm
Forum: LinkIt
Topic: LinkIt ONE SDK for OSX
Replies: 5
Views: 10396

Re: LinkIt ONE SDK for OSX

A Link would be nice.
by sebastian5
Sun May 10, 2015 4:29 am
Forum: LinkIt
Topic: LinkIt ONE SDK for OSX
Replies: 5
Views: 10396

Re: LinkIt ONE SDK for OSX

Got it to work!

Upload works. You just need to press the reset button on the Linkit after every upload.

I used the alternative cdc acm drivers from here:

http://www.mytracks4mac.info/c/index.ph ... yosemite-2
by sebastian5
Sat May 09, 2015 9:49 pm
Forum: LinkIt
Topic: Linkit in Virtual Machine
Replies: 2
Views: 1397

Re: Linkit in Virtual Machine

Sadly I cannot install the Linkit driver with the OSX SDK.
by sebastian5
Sat May 09, 2015 12:30 am
Forum: LinkIt
Topic: LinkIt ONE SDK for OSX
Replies: 5
Views: 10396

Re: LinkIt ONE SDK for OSX

No chance to install that driver.

I use OSX 10.10.3.

I enable Dev Mode (like the readme.txt says).

Then I start the mpkg. It seems to run fine, writes files, etc. but in the end there is always an error message.

"The installation failed.
The installer encountered an error that caused ..."
by sebastian5
Wed Apr 29, 2015 7:37 pm
Forum: LinkIt
Topic: Linkit in Virtual Machine
Replies: 2
Views: 1397

Linkit in Virtual Machine

I run Windows 8.1 in VitualBox on my OSX host. It detects the LinkIt COMs when I insert the USB Cable. I then install the drivers (I did turn off driver signature enforcement). But: nothing happens. Like the drivers werent installed. The Device Manager still shows two unknown COM (Unknown Devices).