Search found 5 matches

by hauke
Thu May 07, 2015 10:16 pm
Forum: Shields
Topic: GPRS shield v2 Arduino Mega error
Replies: 3
Views: 1645

Re: GPRS shield v2 Arduino Mega error

It is possible that all you have to do is go into Suli.cpp and remove the six "return " statements in uart_write_int and uart_write_float. Haven't tested.
by hauke
Thu May 07, 2015 10:12 pm
Forum: Shields
Topic: GPRS shield v2 Arduino Mega error
Replies: 3
Views: 1645

Re: GPRS shield v2 Arduino Mega error

Compiling for Uno works without error (except for low memory warning).
by hauke
Thu May 07, 2015 10:12 pm
Forum: Shields
Topic: GPRS shield v2 Arduino Mega error
Replies: 3
Views: 1645

Re: GPRS shield v2 Arduino Mega error

I have the same issue.
by hauke
Mon Mar 23, 2015 6:38 pm
Forum: Shields
Topic: Programming multiple NODE for CAN BUS SHEILD ?
Replies: 17
Views: 17813

Re: Programming multiple NODE for CAN BUS SHEILD ?

I am correcting my last post. I am addressing pin 8 and can toggle with a digitalWrite.

However, the voltage is only 1.5 V and the LED without a resistor only blinks faintly. Is the shield consuming so much power that there is only very little left?
by hauke
Mon Mar 23, 2015 6:20 pm
Forum: Shields
Topic: Programming multiple NODE for CAN BUS SHEILD ?
Replies: 17
Views: 17813

Re: Programming multiple NODE for CAN BUS SHEILD ?

Hi Loovee,

I am trying to trigger an action on the receiver side, but I cannot even get an LED to blink. I copied your receiver source code. Does it blink the LED for you? In my case, LED on pin 13 (or any other) remains dark.

Do you have any ideas? Thanks!

Hauke