Search found 19 matches

by yokonav
Tue Sep 17, 2019 9:07 am
Forum: New Product Ideas
Topic: NEW Releasing: STM32MP157C Development Board and Look forward to your ideas!
Replies: 27
Views: 11434

Re: NEW Releasing: STM32MP157C Development Board and Look forward to your ideas!

Yes I liked it! That's cool! When can we expect to try out the board? We are debugging the first batch sample, and will make some amendment to it. For example, it is not easy to get the mcu with firmware already flashed for ST-Link, we may consider removing ST-Link. If everything goes well, we can ...
by yokonav
Tue Sep 03, 2019 3:35 am
Forum: New Product Ideas
Topic: Call 4 Inputs for our New Lipo Rider Plus Plus
Replies: 8
Views: 2237

Re: Call 4 Inputs for our New Lipo Rider Plus Plus

I would say the upgraded version a "Lipo Rider Ultra". I would like to see:
1. 3V
2. Protection circuit
3. Reasonable price
4. Headers to power breadboard or other microcontrollers
by yokonav
Wed Aug 21, 2019 6:35 pm
Forum: New Product Ideas
Topic: NEW Releasing: STM32MP157C Development Board and Look forward to your ideas!
Replies: 27
Views: 11434

Re: NEW Releasing: STM32MP157C Development Board and Look forward to your ideas!

Yes I liked it! That's cool! When can we expect to try out the board?
by yokonav
Tue Aug 13, 2019 11:57 am
Forum: New Product Ideas
Topic: Grove AI Hat UART Issues
Replies: 1
Views: 1109

Grove AI Hat UART Issues

RPI 3B+ is powered using 2.5A/5V adapter.and is attached to the Grove AI Hat. The J4 toggle button is ON so the Grove AI Hat gets power from the RPI. The CH340 UART port is not showing in the Arduino IDE or by using ls -l /dev/tty.*. When I power the Grove AI Hat directly and keep the J4 toggle butt...
by yokonav
Fri Aug 09, 2019 1:28 pm
Forum: New Product Ideas
Topic: New Product Idea: Teensy 4.0 Grove Shield
Replies: 1
Views: 1015

New Product Idea: Teensy 4.0 Grove Shield

Now Teensy 4.0 is out and it would be really great to see grove shield for it. I think the shield could be back-compatible with the Teensy 3.2/3.6 as they have same form factor.
by yokonav
Tue Aug 06, 2019 9:47 am
Forum: New Product Ideas
Topic: New Product Idea: Spresense Grove Shield
Replies: 0
Views: 1023

New Product Idea: Spresense Grove Shield

The Sony Spresense is a promising development board. It would be nice to have a Grove Shield for Spresense.
by yokonav
Sat Jul 06, 2019 7:39 am
Forum: New Product Ideas
Topic: New Product Idea: An FPGA Development board- Spartan Edge Accelerator Board
Replies: 12
Views: 7188

Re: New Product Idea: An FPGA Shield for Arduino- Spartan Edge Accelerator Board

I am a bit confused... why Arduino shield? Since this board has almost everything, I think this board itself can be an Arduino-compatible board with the onboard ESP32. As an added benefit, MicroPython can also be used. The groves and LEDs position is OK but when you stack a shield on the top of this...