Search found 4 matches
- Wed Mar 18, 2015 3:23 am
- Forum: LinkIt
- Topic: Grove Button
- Replies: 1
- Views: 1911
Grove Button
Hi, I can't get the Grove Button to work with the Linkit One. I've configured the pin as a input and tried with many different pins. The digitalRead command always returns a 1 and if I've pull the pin to ground I get a 0. When measuring the voltage over the pin and I get 2.25 V. I think the pins are...
Led bar
Hi,
I'm using the led bar in combination with the LinkIt one and it works on 3.3V but when I've set the Grove Shield to 5V it stops working.
I've tested the ledbar on a Intel Edison and there it works on 5V.
What's the reason behind this? How can i fix it?
Kind regards,
Frederik
I'm using the led bar in combination with the LinkIt one and it works on 3.3V but when I've set the Grove Shield to 5V it stops working.
I've tested the ledbar on a Intel Edison and there it works on 5V.
What's the reason behind this? How can i fix it?
Kind regards,
Frederik
- Fri Jan 09, 2015 5:05 am
- Forum: LinkIt
- Topic: Can't upload sketch
- Replies: 2
- Views: 1843
Re: Can't upload sketch
I've went to the steps below and got the board working again:
1. Does the switches on the right side, (MS & USB)
2. Choose the right COM Port(MTK USB DEBUG PORT)
3. Update the firmware and try again
4. Try another PC
5. Try another USB cable
(Got them from support)
1. Does the switches on the right side, (MS & USB)
2. Choose the right COM Port(MTK USB DEBUG PORT)
3. Update the firmware and try again
4. Try another PC
5. Try another USB cable
(Got them from support)
- Tue Jan 06, 2015 8:30 pm
- Forum: LinkIt
- Topic: Can't upload sketch
- Replies: 2
- Views: 1843
Can't upload sketch
Hi, I've updated the LinkIt SDK to the 1.0.42 and the firmware of the LinkIt One. Since then i'm unable to upload any code to the LinkIt One. In VS 2013 via Visual Micro I get the error "The uploader returned an error" after the pushtool.exe gets called. The arduino IDE keeps uploading the code. The...