Search found 3 matches

by mail26
Sun May 08, 2016 3:36 am
Forum: Arduino & Seeeduino
Topic: Seeeduino Stalker v3, PCB Jumper Pad "D13_LED" not working
Replies: 0
Views: 2234

Seeeduino Stalker v3, PCB Jumper Pad "D13_LED" not working

Beside the Known Issue http://www.seeedstudio.com/wiki/Seeeduino-Stalker_v3#Known_Issue it seems that the "D13_LED" PCB Jumper Pads has an error and was designed wrong. In the Eagle file (board view) is one pad with no connection! So cutting the trace has no effect. Don't know why so a sloppy error ...
by mail26
Tue Jan 06, 2015 5:38 pm
Forum: Arduino & Seeeduino
Topic: Connecting 2 Grove devices to Stalker 3.0
Replies: 11
Views: 6229

Re: Connecting 2 Grove devices to Stalker 3.0

Are you using this DHTxx breakout: http://www.seeedstudio.com/wiki/Grove-_Temperature_and_Humidity_Sensor so you can have a look at the first photo: You can see the pin connections: The order is GND VCC NC SIG NC means not connected and SIG is your signal, so the last pin is the signal pin. Compare ...
by mail26
Tue Jan 06, 2015 5:10 pm
Forum: Arduino & Seeeduino
Topic: Stalker V3 compatibility with Same box as V2.3?
Replies: 3
Views: 1860

Re: Stalker V3 compatibility with Same box as V2.3?

Is only the case compatible or also the mounting holes?