Search found 27 matches

by matthew
Tue Apr 28, 2015 6:18 pm
Forum: LinkIt
Topic: LSMS class implementation of Stream is non-standard
Replies: 0
Views: 3913

LSMS class implementation of Stream is non-standard

Hi, I am writing a general SMS library to reliably send and receive long messages, with re-sequencing and lost msg recovery. However while LSMS extends from Stream, it does not implement available() in the expected and standard stream manner. LSMS uses available() to indicate that a SMS message is a...
by matthew
Wed Apr 01, 2015 11:34 am
Forum: LinkIt
Topic: Changing Networks without reprogramming - pfodWifiConfigV1
Replies: 1
Views: 4212

Re: Changing Networks without reprogramming - pfodWifiConnec

Changed name to pfodWifiConfigV1 and added Android app available from Googleplay or SlideMe if you don't have GooglePlay support on your Android mobile.
by matthew
Fri Mar 20, 2015 6:34 am
Forum: LinkIt
Topic: Question about LinkIt ONE wifi security
Replies: 1
Views: 1317

Question about LinkIt ONE wifi security

LinkIt ONE has wifi security option of WPA, is this WPA or WPA2 or both?
if it is really WPA2 does it use AES security?
by matthew
Thu Mar 05, 2015 5:29 pm
Forum: LinkIt
Topic: linkit one wifi + analog sensor
Replies: 3
Views: 2019

Re: linkit one wifi + analog sensor

see
http://www.seeedstudio.com/forum/viewto ... =42&t=5750

for a solution to the
m_password(NULL)
problem
by matthew
Thu Mar 05, 2015 5:24 pm
Forum: LinkIt
Topic: Changing Networks without reprogramming - pfodWifiConfigV1
Replies: 1
Views: 4212

Changing Networks without reprogramming - pfodWifiConfigV1

This post introduces pfodWifiConfigV1 for Linkit ONE. pfodWifiConfigV1 lets your user connect your LinkIt ONE to their network without you having to program in their network SSID and password. See http://www.forward.com.au/pfod/pfodWifiConfig/index.html for the details and a link to the LinkIt ONE t...
by matthew
Tue Feb 03, 2015 5:48 pm
Forum: LinkIt
Topic: Code Generator for LinkItONE
Replies: 11
Views: 13767

Re: Code Generator for LinkItONE

I have published a pfodLinkIt library for LinkIt ONE. The library handles Bluetooth and Wifi connections with optional 128 bit security. see http://www.forward.com.au/pfod/pfodParserLibraries/index.html I have also updated the free pfodDesigner V1.2.573, to work with this library when you generate c...
by matthew
Sun Feb 01, 2015 4:58 pm
Forum: LinkIt
Topic: Code Generator for LinkItONE
Replies: 11
Views: 13767

Re: Code Generator for LinkItONE

Changed to using EEPROM library to remove the above compile error. Two problems i) #include <EEPROM.h> does not work in my .cpp file inside my library directory libraries/pfodParser ... I need to put a copy of this include in the main sketch to get the pre-processing to set up the correct include pa...
by matthew
Sun Feb 01, 2015 4:35 pm
Forum: LinkIt
Topic: EEPROM.h: No such file or directory
Replies: 1
Views: 2686

Re: EEPROM.h: No such file or directory

#include <LEEPROM.h>
works but this is non-standard for Arduino compatibility and breaks standard sketches.
by matthew
Sun Feb 01, 2015 4:16 pm
Forum: LinkIt
Topic: EEPROM.h: No such file or directory
Replies: 1
Views: 2686

EEPROM.h: No such file or directory

Tried compiling this code from the docs #include <EEPROM.h> void setup() { // put your setup code here, to run once: } void loop() { // put your main code here, to run repeatedly: byte a = 1; EEPROM.write(0, a); byte b = EEPROM.read(0); if (a == b) { // do something. delay(2000); } } Would not compi...
by matthew
Sun Feb 01, 2015 8:00 am
Forum: LinkIt
Topic: Code Generator for LinkItONE
Replies: 11
Views: 13767

Re: Code Generator for LinkItONE

I am now working on SMS connections to LinkIt ONE. As preparation I have modified pfodSecurity library to remove all the Atmel 8bit AVR assembler and replace it with C code. However I have now come across another issue. How to access eeprom on LinkIt ONE As part of the security (see http://www.forwa...