Search found 4 matches

by frederickmartinez
Tue Dec 08, 2015 10:37 am
Forum: Wearables
Topic: Need help with RX/TX thread on HM-11 Android application
Replies: 0
Views: 2411

Need help with RX/TX thread on HM-11 Android application

Since the HMCommAssist is not open source and I need to have directional communication with the Arduino and Android. I am willing to share the code if someone can help with the issue I am having. The issue I am having created a thread but now I can not transmit data to the arduino. Post a reply if y...
by frederickmartinez
Wed Jan 14, 2015 10:21 am
Forum: Wearables
Topic: Xadow BLE Android Source
Replies: 1
Views: 1752

Xadow BLE Android Source

I am looking for Android code that will work with the Xadow BLE module (serial). The only app that I have downloaded that works with the Xadow is HMBLE com Assistant. This app is not open source so I can not make any updates. How can a company sell device without any open source code to go along wit...
by frederickmartinez
Wed Jan 14, 2015 10:13 am
Forum: Wearables
Topic: Xadow establishing BLE Slave wo computer
Replies: 3
Views: 2353

Re: Xadow establishing BLE Slave wo computer

fixed it by removing the following code:

while (!Serial.available());
Serial1.print("AT+ROLE0"); // Sets the bluetooth module as a slave but doesn't work
by frederickmartinez
Wed Dec 17, 2014 12:13 am
Forum: Wearables
Topic: Xadow establishing BLE Slave wo computer
Replies: 3
Views: 2353

Xadow establishing BLE Slave wo computer

How do I resolve the issue the device must be connected to the computer via usb port and "AT + ROLE0" command must be entered on Arduino serial monitor page in order to establish the BLE communication on the device as a slave. if you power down the device via a battery switch you must go thru the sa...