Search found 14 matches

by back_kevin
Sun Apr 12, 2015 10:36 pm
Forum: LinkIt
Topic: Powerup the Linkit one
Replies: 1
Views: 1547

Powerup the Linkit one

hi on arduino boards there are a VIN pin for external Power is there a way to powerup my linkit one without the usb i try to connect my arduino mega to linkit one the power from arduino comme from accu go to VIN i connect : 5V arduino to Linkit one 5V 3.3V arduino to Linkit one 3.3V GND arduino to L...
by back_kevin
Wed Mar 18, 2015 4:43 am
Forum: LinkIt
Topic: Grove Button
Replies: 1
Views: 1832

Re: Grove Button

hi

the grove bp don`t works

i have the same probleme keep your sketch and change the bp to Touch Sensor
and try now this works
by back_kevin
Tue Mar 17, 2015 9:46 pm
Forum: LinkIt
Topic: Terrarium controled by Linkit ONE
Replies: 3
Views: 1917

Re: Terrarium controled by Linkit ONE

yes i can share it later (at version 1.0)

at the moment i try to kill last bugs in the sketch

i have a big problem with the wifi connection it is not stable

after x time i can`t reconnect to server
by back_kevin
Wed Mar 11, 2015 1:44 am
Forum: LinkIt
Topic: Terrarium controled by Linkit ONE
Replies: 3
Views: 1917

Terrarium controled by Linkit ONE

HI here is my new project : controle my terrarium with Linkit ONE: features: -control the water in the tank (if to low switch all water tools off)----------------------------------in progress -control the humidity (if over 70% switch foger off )-----------------------------------------------ok -cont...
by back_kevin
Wed Dec 17, 2014 3:43 am
Forum: LinkIt
Topic: how to run DHTXXX
Replies: 3
Views: 3601

Re: how to run DHTXXX

no it don`t work

the first problem is the sensor is digital and not analoge

i found now a lib that works fine i connect my sensors to grove shield D3 and D4
by back_kevin
Sun Dec 14, 2014 12:16 am
Forum: Grove
Topic: GROVE LED BAR
Replies: 1
Views: 933

GROVE LED BAR

hi why the led bar don`t run under 5Vdc?

my code works under 3,3v but under 5v the bar don`t run

in doc is written power from 3,3 to 5 Vdc
by back_kevin
Sat Dec 13, 2014 4:17 am
Forum: LinkIt
Topic: Serial not working
Replies: 7
Views: 6035

Re: Serial not working

look into the forum

under can`t run wifi and gprs

add 2 lines into the sketch and you see your serial
by back_kevin
Thu Dec 11, 2014 11:04 pm
Forum: LinkIt
Topic: how to run DHTXXX
Replies: 3
Views: 3601

how to run DHTXXX

hi i have a new problem i want to use 2 dht 11 on my grove shield V2.0 what for a library i need to do this ? i try with the grove library from wiki page http://www.seeedstudio.com/wiki/Grove_-_Temperature_and_Humidity_Sensor but i get errors when i compile it : In file included from DHTtester.ino:4...
by back_kevin
Wed Dec 10, 2014 7:26 am
Forum: LinkIt
Topic: can`t run wifi or gprs server
Replies: 6
Views: 4212

Re: can`t run wifi or gprs server

hi i try at the moment this code: #include <LTask.h> #include <LWiFi.h> #include <LWiFiServer.h> #include <LWiFiClient.h> #define WIFI_AP "BACK_HOME_1" #define WIFI_PASSWORD "556890556890" #define WIFI_AUTH LWIFI_WPA// choose from LWIFI_OPEN, LWIFI_WPA, or LWIFI_WEP according to your WiFi AP configu...
by back_kevin
Mon Dec 08, 2014 8:54 pm
Forum: LinkIt
Topic: can`t run wifi or gprs server
Replies: 6
Views: 4212

Re: can`t run wifi or gprs server

ok the probleme was the cache in firefox

but how can i add a button to the html part to control a led