Search found 11 matches

by wenjie.zhang
Fri Feb 27, 2015 6:46 pm
Forum: Arduino & Seeeduino
Topic: Stalker 2.3 & 3 and elecrow HC-5 bluetooth bee 2.0
Replies: 4
Views: 2810

Re: BOUNTY: stalker 2.3 & 3 and elecrow HC-5 bluetooth bee 2

Hi friends, There are two points need to be explained about your problem: 1.It isn't a conflict that both UartSBee and Bee socket use the same pins (0 & 1 ) as communication port. UartSBee is used as a programmer for Seeeduino Stalker. You can remove Bluetooth Bee when uploading with UartSBee, then ...
by wenjie.zhang
Wed Jan 07, 2015 8:15 pm
Forum: To Be Classified
Topic: Li-Po Rider: how do you unplug the battery safely?
Replies: 2
Views: 4232

Re: Li-Po Rider: how do you unplug the battery safely?

Hi,

I suggest you to plug and unplug the JST connector quickly and repeatly to make the connector more smoother.Then maybe you will find it more easier to unplug it.

Wish you good luck!
by wenjie.zhang
Wed Jan 07, 2015 6:11 pm
Forum: Bee series & WSN
Topic: RFBee and transmission distance
Replies: 3
Views: 2745

Re: RFBee and transmission distance

Hi friends, The max transmit range of the RFBee is listed below: Indoor/Urban: up to 50m Outdoor line-of-sight: up to 120m Maybe you can try using the AT command "PA" to increase the transmitting power, thus expanding the transmit range. For the use of AT command,refer to the file "RFBee User Manual...
by wenjie.zhang
Tue Dec 16, 2014 2:04 pm
Forum: Grove
Topic: Grove PIR 1.2 Potentiometer
Replies: 2
Views: 1362

Re: Grove PIR 1.2 Potentiometer

Hi,friend!

The Potentiometer isn't included in the Sensor now.Sorry for not correcting the information in time.
by wenjie.zhang
Sat Nov 22, 2014 11:23 am
Forum: Grove
Topic: Grove - Alcohol Sensor protocol & address
Replies: 1
Views: 2664

Re: Grove - Alcohol Sensor protocol & address

Hi friends,

Sorry for replying so late.
The Grove - Alcohol Sensor is an analog sensor,you should plug it to the analog connector(J7 or J8) of Grove - Base Shield for IOIO-OTG. Here is the more detailed imformation:http://www.seeedstudio.com/wiki/index.p ... hol_Sensor
by wenjie.zhang
Fri Nov 21, 2014 12:48 pm
Forum: Grove
Topic: Grove on Hercules platform.
Replies: 1
Views: 939

Re: Grove on Hercules platform.

Hi,

You can find more detailed imformation in our wiki page,here is the related link:http://www.seeedstudio.com/wiki/Grove_-_GPS
Hope it is useful for you!
by wenjie.zhang
Thu Nov 20, 2014 5:56 pm
Forum: Grove
Topic: Moisture sensor - LEAD FREE
Replies: 1
Views: 1234

Re: Moisture sensor - LEAD FREE

Hi,

Please feel relieved the use, all of our products are manufactured according to the standard of RoHS.
by wenjie.zhang
Thu Nov 20, 2014 3:11 pm
Forum: Grove
Topic: 4WD Robot Controller & I2C bus
Replies: 3
Views: 1910

Re: 4WD Robot Controller & I2C bus

Hi Perri,

I'm sorry to tell you that the Controller Board can not be programmed with Arduino YUN for which does't have a FTDI chip. So please be patient and wait.
by wenjie.zhang
Wed Nov 19, 2014 5:00 pm
Forum: Grove
Topic: Grove PH Sensor SKU: SEN00600P
Replies: 1
Views: 2013

Re: Grove PH Sensor SKU: SEN00600P

Hi ajroche,

Please check whether there's any conflict on the hardware connection and the code. This large ranging values probably were caused by unstable serial data transferring. If you would like, you can also send us your code and the data output. Thank you!
by wenjie.zhang
Wed Nov 19, 2014 3:19 pm
Forum: Grove
Topic: 4WD Robot Controller & I2C bus
Replies: 3
Views: 1910

Re: 4WD Robot Controller & I2C bus

Hi Perri,

The Grove connector is used to connect with servo, encoder and sensors. For more detailed information, please visit our Wiki, here is the related link:http://www.seeedstudio.com/wiki/Hercule ... #Resources