Search found 39 matches

by xuguang.shao
Tue Jan 21, 2020 3:32 pm
Forum: ReSpeaker
Topic: ReSpeaker USB Mic Array AEC tuning?
Replies: 3
Views: 474

Re: ReSpeaker USB Mic Array AEC tuning?

The solution of ReSpeaker USB Mic Array - XMOS3000 is for mono-playback use only. The acoustic characteristic between stereo and mono is different enough for XMOS3000 to exceed its tolerance, especially when you use powerful speakers. More deeply, the differences lie in: 1. mix in digital (even in a...
by xuguang.shao
Fri Aug 24, 2018 4:33 pm
Forum: Grove
Topic: ControlMotoDriver - calling method is crashing the whole app
Replies: 9
Views: 3171

Re: ControlMotoDriver - calling method is crashing the whole app

I've successfully driven the Grove - Mini I2C Motor Driver, and there's no same issue reported for this, so I can temporarily conclude that your issue isn't a common one. We've done some research and tried out some methods Could you share more informations about your research? Have you tried other I...
by xuguang.shao
Thu Aug 09, 2018 8:20 pm
Forum: Grove
Topic: ControlMotoDriver - calling method is crashing the whole app
Replies: 9
Views: 3171

Re: ControlMotoDriver - calling method is crashing the whole app

Hi Nace, Is there any possiblity that application is crashing because using wrong port on the GrovePi+? No, the I2C Grove doesn't care which I2C port you're connecting it to, your problem might be caused by bad network communication to the Azure, in which case the program will throw an exception whi...
by xuguang.shao
Thu Aug 09, 2018 8:11 pm
Forum: Grove
Topic: Grovepi starter for windows 10 iot core based on raspberry pi
Replies: 2
Views: 1206

Re: Grovepi starter for windows 10 iot core based on raspberry pi

I don't think @papeyorogadiaga's problem is the one I'm trying to solve https://github.com/Seeed-Studio/AzureGroveKit/issues/2 @papeyorogadiaga, the GrovePi official examples all work good, please dig around to know how to run Dexter's GrovePi C# examples I can give you a brief, but the rest is the ...
by xuguang.shao
Wed May 04, 2016 12:18 pm
Forum: Wio Series
Topic: How to get events from accelerometer
Replies: 10
Views: 4330

Re: How to get events from accelerometer

Oh by the way, your project sounds really fancy! especially the solar charging part :D
by xuguang.shao
Wed May 04, 2016 12:16 pm
Forum: Wio Series
Topic: How to get events from accelerometer
Replies: 10
Views: 4330

Re: How to get events from accelerometer

Hi bjarne, We were planning to provide coding assist in the web based frontend. For now, you have to find the functions in source code here https://github.com/Seeed-Studio/Grove_Drivers_for_Wio and find the class instance name with any of the following method a) API call curl https://iot.seeed.cc/v1...
by xuguang.shao
Tue May 03, 2016 11:16 pm
Forum: Wio Series
Topic: How to get events from accelerometer
Replies: 10
Views: 4330

Re: How to get events from accelerometer

Hi all, Thank you for advising and good discussion here. Yes, it's easy for us to add event for particular grove. But the limitation we have here is that the grove system can only transfer interrupt to host MCU with GPIO line(either I2C nor UART). All I2C groves will have to drop the interrupt info ...
by xuguang.shao
Wed Apr 27, 2016 11:33 am
Forum: Wio Series
Topic: #Discussion#Wio Link Server document has released, then?
Replies: 4
Views: 2542

Re: #Discussion#Wio Link Server document has released, then?

Hi philip, Python version is fine. The problem is your earlier installation is still running (at the same machine), and listening at port 8080. Unfortunately 8080 is used by lean server too. The full function server has "data exchange function" as well, so we assume that there is no need to deploy a...
by xuguang.shao
Mon Apr 25, 2016 2:02 pm
Forum: Wio Series
Topic: Reading Wio with Processing
Replies: 8
Views: 2424

Re: Reading Wio with Processing

Hi,

Basically it's because Java do not recognize the Root CA. Which server are you connecting? According to this workaround http://magicmonster.com/kb/prg/java/ssl ... ailed.html, I can give you the Root CA and some further steps need to be done by you.
by xuguang.shao
Mon Apr 25, 2016 1:43 pm
Forum: Wio Series
Topic: Can't connect to a newly deployed server
Replies: 1
Views: 1484

Re: Can't connect to a newly deployed server

Hi, Are u using the iOS app? That error is thrown when the app cant find the existence of the newly added wio or the app cant connect to the server. It seems your app does connect to the server because you successfully created your account and logged into the server. So the problem happens in the Wi...