Search found 2 matches

by testasecc
Fri May 17, 2019 3:00 pm
Forum: Shields
Topic: CAN BUS Shield V2 reception Issue
Replies: 1
Views: 1033

Re: CAN BUS Shield V2 reception Issue

// include libraries #include <mcp_can.h> #include <mcp_can_dfs.h> //--------------------------- // // Variable initialisation // //--------------------------- #define VAR_TURN 1350 #define NEUTRAL 40 #define ACT_VAR 500 #define MAX_COMMAND 220 //90% of 255 #define MIN_COMMAND 30 //10% of 255 #defi...
by testasecc
Thu May 16, 2019 3:08 pm
Forum: Shields
Topic: CAN BUS Shield V2 reception Issue
Replies: 1
Views: 1033

CAN BUS Shield V2 reception Issue

Dear All, I am a newbie on arduino project with CAN communication so I would like to get your comments on an issue that is blocking me. This project is a vehicule with 4 motors 2 are for the direction and 2 are for the traction. The motors are driven by various controllers (maxon controllers for the...