Indeed, on the first attempts I was in oversampling mode. But when I deleted all files and put back the WPT-backup, I wasn't anymore after startup. You see in my screenshots, that I already wasn't at that time (buffer is not red anymore).
I'm using wildcats community app 4.4 (HW V2.70 Sys Ver 1.52) and have problems with calibration. I did the calibration (with the different voltages for each of the 8 ranges) a couple of times for LOW and HIGH BATTERY and saved it , but the measuring still doesn't work right. I also deleted all files...
Thank you rimidalv007! Good job! Single shot works! Now this DSO is usable to me. Unfortunatly, I cannot set/reduce buffer size on low timebase with this version of Benf Firmware? :( Was it hard to implement the new display driver? Maybe there could be an easy way to disassemble the hex-file of Benf...
Hello, I buy this DSO to measure small things (car electronic, signal emitter, analog sensors / potentiometer, etc.). I cannot use alternative fw (Bootloader 3.26D), so I have to use the original 4.21. I read the manual (it's not very detailed), but I need held to use it: - Neigher Yn FitRange nor X...
Same here. The seller wrote "DSO NANO Hardware 1.6 + Paul's Firmware 1.5". What is Paul's Firmware 1.5? At web I found it's a third party firmware? Where can I get it? Or is Ver4.21 already this "third party" firmware? If so, where can I get the original firmware? Actually I decided to use the Benf ...